<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: The conditions which change to Serial-Download-Mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410196#M61402</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sorry that a reply is delayed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My customer checked that each CD was not Active.&lt;/P&gt;&lt;P&gt;However, their board does not switch over to Serial-Download-Mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if you came up with something our mistake.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Sep 2015 12:44:26 GMT</pubDate>
    <dc:creator>george</dc:creator>
    <dc:date>2015-09-14T12:44:26Z</dc:date>
    <item>
      <title>The conditions which change to Serial-Download-Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410192#M61398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My customer are constructing the manufacturing process of the product using current i.MX6-Solo.&lt;/P&gt;&lt;P&gt;Their product is boot from parallel NOR-Flash via EIM interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When nothing is being written to NOR-flash (all contents 0xFF) in the Internal Boot Mode, We thought that it switches over boot from NOR-flash to Serial-Download-Mode.&lt;/P&gt;&lt;P&gt;However, their board does not switch over to Serial-Download-Mode. &lt;STRONG style="font-size: 8pt;"&gt;*PC does not detect USB-Device.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once writing a program into NOR using Serial-Downloader, of course, the board is correctly boot from NOR-flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Doesn't i.MX6-Solo switch over to Serial-downloader, when reading 0xFF from NOR-Flash in boot?&lt;/P&gt;&lt;P&gt;Do my customer have to change Boot-Mode switch setting on the board in a manufacturing process?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Aug 2015 06:58:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410192#M61398</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2015-08-31T06:58:34Z</dc:date>
    </item>
    <item>
      <title>Re: The conditions which change to Serial-Download-Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410193#M61399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;George, hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If (hardware selected) boot device fails, the i.MX6 can try boot SD / MMC in so called&lt;/P&gt;&lt;P&gt;SD / MMC Manufacture mode before applying to serial (USB) boot.&lt;/P&gt;&lt;P&gt;Please look at section 8.11 (SD/MMC Manufacture Mode) of the&amp;nbsp; IMX6SDLRM (Rev. 2, 04/2015)&lt;/P&gt;&lt;P&gt;for details. It is supported in i.MX6SDL and i.MX6SL. However, it is not available on i.MX6DQ.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, please try to configure BOOT_MODE[1:0] pins for Serial Downloader mode.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Aug 2015 07:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410193#M61399</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-31T07:29:53Z</dc:date>
    </item>
    <item>
      <title>Re: The conditions which change to Serial-Download-Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410194#M61400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the quick reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked Section 8.11.&lt;/P&gt;&lt;P&gt;That is, if SD1_CD and SD2_CD are inactivities in the case of my customer, it will switch over to Serial-download-mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is my understanding correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Aug 2015 08:10:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410194#M61400</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2015-08-31T08:10:12Z</dc:date>
    </item>
    <item>
      <title>Re: The conditions which change to Serial-Download-Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410195#M61401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes.&lt;BR /&gt;Note, &lt;SPAN style="font-size: 10.5pt; font-family: 'Arial','sans-serif'; color: black;"&gt;there are differences between i.MX6SDL and i.MX6SL:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.5pt; font-family: 'Arial','sans-serif'; color: black;"&gt;In MX6SDL both SD1 and SD2 are used for Manufacturing, the pins used for SD1_CD is GPIO_1 and SD2_CD is GPIO_4&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.5pt; font-family: 'Arial','sans-serif'; color: black;"&gt;In MX6SL only SD1 is used for CD, the pin used for CD signal is KEY_ROW7"&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.5pt; font-family: 'Arial','sans-serif'; color: black;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Aug 2015 09:51:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410195#M61401</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-31T09:51:37Z</dc:date>
    </item>
    <item>
      <title>Re: The conditions which change to Serial-Download-Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410196#M61402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sorry that a reply is delayed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My customer checked that each CD was not Active.&lt;/P&gt;&lt;P&gt;However, their board does not switch over to Serial-Download-Mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if you came up with something our mistake.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Sep 2015 12:44:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410196#M61402</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2015-09-14T12:44:26Z</dc:date>
    </item>
    <item>
      <title>Re: The conditions which change to Serial-Download-Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410197#M61403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;George, hi !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Do my customer have to change Boot-Mode switch setting on the board in a manufacturing process?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Looks like this is the only solution for the case.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 02:50:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410197#M61403</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-09-18T02:50:22Z</dc:date>
    </item>
    <item>
      <title>Re: The conditions which change to Serial-Download-Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410198#M61404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Umm.. I think so too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, my customer feels uneasy.&lt;/P&gt;&lt;P&gt;The behavior differs from the behavior imagined in the design.&lt;/P&gt;&lt;P&gt;They are hesitating at the mass-production start, leaving an issue on their board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me check once again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the available data for boot are not got from NOR-Flash, does it switch over to SD/MMC Manufacture Mode or Serial Download mode.&lt;/P&gt;&lt;P&gt;Is this correct as device behavior?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 05:29:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-conditions-which-change-to-Serial-Download-Mode/m-p/410198#M61404</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2015-09-18T05:29:21Z</dc:date>
    </item>
  </channel>
</rss>