<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX287 running on external oscillator? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX287-running-on-external-oscillator/m-p/409890#M61338</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The internal oscillator may be used in low power mode. By default it is disabled.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Jun 2015 09:31:55 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-06-18T09:31:55Z</dc:date>
    <item>
      <title>iMX287 running on external oscillator?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX287-running-on-external-oscillator/m-p/409887#M61335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to make the iMX work with external oscillator (not crystal)? We are discussing this alternative because integrated oscillators offer much better MTBF values than crystals. (20 times better!)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not, can we run the iMX (including the RTC subcircuit) only with the internal oscillator?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bets regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2015 07:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX287-running-on-external-oscillator/m-p/409887#M61335</guid>
      <dc:creator>albertguardiola</dc:creator>
      <dc:date>2015-06-18T07:57:34Z</dc:date>
    </item>
    <item>
      <title>Re: iMX287 running on external oscillator?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX287-running-on-external-oscillator/m-p/409888#M61336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am afraid, we have no any specifications for using external clock sources,&lt;/P&gt;&lt;P&gt;except crystals, with i.MX28.&amp;nbsp; The only recommendations are to use 24MHz, 30ppm&lt;/P&gt;&lt;P&gt;Crystal, and 32kHz, 20ppm Crystal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;More details for 24Mhz :&lt;/P&gt;&lt;P&gt;+/- 30ppm ;&lt;/P&gt;&lt;P&gt;max ESR: ~50ohm ;&lt;/P&gt;&lt;P&gt;Load capacitor : 10pf-15pf ;&lt;/P&gt;&lt;P&gt;Shunt capacitor : 5pf-7pf.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Sorry, an external oscillator option has never been tested with i.MX28.&lt;/P&gt;&lt;P&gt;Theoretically, it seems to be possible to apply an external 24MHz clock signal&lt;/P&gt;&lt;P&gt;to XTALI and leave XTALO open, however, the amplitude of an external clock&lt;/P&gt;&lt;P&gt;signal must not exceed VDDXTAL, that is typically around 1.0V.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The internal oscillator may be used in low power mode. By default it is disabled.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2015 09:14:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX287-running-on-external-oscillator/m-p/409888#M61336</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-06-18T09:14:49Z</dc:date>
    </item>
    <item>
      <title>Re: iMX287 running on external oscillator?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX287-running-on-external-oscillator/m-p/409889#M61337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks indeed, Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How about running the whole IMX on internal oscillator? Is there any limitation in functionality?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I cannot find literature on the internal oscillator in the datasheets: could you provide quality specs on it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2015 09:22:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX287-running-on-external-oscillator/m-p/409889#M61337</guid>
      <dc:creator>albertguardiola</dc:creator>
      <dc:date>2015-06-18T09:22:13Z</dc:date>
    </item>
    <item>
      <title>Re: iMX287 running on external oscillator?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX287-running-on-external-oscillator/m-p/409890#M61338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The internal oscillator may be used in low power mode. By default it is disabled.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2015 09:31:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX287-running-on-external-oscillator/m-p/409890#M61338</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-06-18T09:31:55Z</dc:date>
    </item>
    <item>
      <title>Re: iMX287 running on external oscillator?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX287-running-on-external-oscillator/m-p/409891#M61339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the info, Yuri. Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2015 12:49:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX287-running-on-external-oscillator/m-p/409891#M61339</guid>
      <dc:creator>albertguardiola</dc:creator>
      <dc:date>2015-06-18T12:49:02Z</dc:date>
    </item>
  </channel>
</rss>