<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PF0100 Charging Issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-Charging-Issue/m-p/409673#M61250</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the SABRE SDB and I placed a coin cell battery on the board, but it doesn't charge the battery.&amp;nbsp; When the battery is initially placed (with a charge) the RTC works as intended, but when battery discharges and power is plugged in, the PF0100 is not charging.&amp;nbsp; Could it be that by default the PF0100 does not have the COINCHEN bit enabled in the COINCTL register?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Joseph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jul 2015 14:38:36 GMT</pubDate>
    <dc:creator>Jochi119</dc:creator>
    <dc:date>2015-07-14T14:38:36Z</dc:date>
    <item>
      <title>PF0100 Charging Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-Charging-Issue/m-p/409673#M61250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the SABRE SDB and I placed a coin cell battery on the board, but it doesn't charge the battery.&amp;nbsp; When the battery is initially placed (with a charge) the RTC works as intended, but when battery discharges and power is plugged in, the PF0100 is not charging.&amp;nbsp; Could it be that by default the PF0100 does not have the COINCHEN bit enabled in the COINCTL register?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Joseph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2015 14:38:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-Charging-Issue/m-p/409673#M61250</guid>
      <dc:creator>Jochi119</dc:creator>
      <dc:date>2015-07-14T14:38:36Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 Charging Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-Charging-Issue/m-p/409674#M61251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joseph&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes you are right, also one needs to set VCOIN -Coin cell charger output voltage&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53767i94A9D9BC6F37740B/image-size/large?v=v2&amp;amp;px=999" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 02:34:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-Charging-Issue/m-p/409674#M61251</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-15T02:34:23Z</dc:date>
    </item>
  </channel>
</rss>