<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX53 ENGcm11135.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-ENGcm11135/m-p/409663#M61247</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;correct!, system should have an active process in secure state, That the reason that init.s includes Write the Cache Size selection register, as published &lt;/P&gt;&lt;P data-canvas-width="289.8424941176471" style="font-size: 16.8235px; font-family: serif;"&gt;sequence for cleaning the entire cache, it save the CSSELR and then restore it value, corresponding to the security state the processor is transitioning.&lt;/P&gt;&lt;P data-canvas-width="289.8424941176471" style="font-size: 16.8235px; font-family: serif;"&gt;Please take in mind that,&amp;nbsp; The specified behavior and that can limit or severely impair the intended use of specified features, but does not render the product unusable in all or the majority of applications&lt;/P&gt;&lt;P data-canvas-width="289.8424941176471" style="font-size: 16.8235px; font-family: serif;"&gt;&lt;/P&gt;&lt;P data-canvas-width="289.8424941176471" style="font-size: 16.8235px; font-family: serif;"&gt;Hope this helps&lt;/P&gt;&lt;P data-canvas-width="289.8424941176471" style="font-size: 16.8235px; font-family: serif;"&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Jun 2015 15:10:59 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2015-06-02T15:10:59Z</dc:date>
    <item>
      <title>i.MX53 ENGcm11135.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-ENGcm11135/m-p/409662#M61246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;Our patner have a question about i.MX53 ENGcm11135.&lt;BR /&gt;Pleas see the "WinCE BSP Status" in IMX53CE Rev.5.&lt;BR /&gt;It says " System does not perform cache maintenance in non-secure mode".&lt;BR /&gt;But they found CSSELR setting in the following WCE700_MX53_ER_1105 source codes.&lt;/P&gt;&lt;P&gt;=====&lt;BR /&gt;platform\common\src\soc\COMMON_FSL_V3\OAL\ARMV7\CACHE\init.s(42):&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mcr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; p15, 2, r3, C0, C0, 0&amp;nbsp;&amp;nbsp; ; Write the Cache Size selection register&lt;BR /&gt;platform\common\src\soc\COMMON_FSL_V3\OAL\ARMV7\CACHE\init.s(81):&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mcr&amp;nbsp;&amp;nbsp; p15, 2, r3, C0, C0, 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; Write the Cache Size selection register&lt;BR /&gt;platform\common\src\soc\COMMON_FSL_V3\OAL\ARMV7\CACHE\init.s(116):&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mcr&amp;nbsp;&amp;nbsp; p15, 2, r3, c0, c0, 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; Write the Cache Size selection register&lt;BR /&gt;platform\common\src\soc\COMMON_FSL_V3\OAL\ARMV7\CACHE\init.s(155):&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mcr&amp;nbsp;&amp;nbsp; p15, 2, r3, c0, c0, 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; Write the Cache Size selection register&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;platform\iMX53_SMD\SRC\OAL\OALLIB\startup.s(833):&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mcr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; p15, 2, r10, c0, c0, 0&amp;nbsp; ; Write the Cache Size selection register&lt;BR /&gt;=====&lt;/P&gt;&lt;P&gt;I think the above CSSELR setting is executed in secure mode, so it is no problem.&lt;BR /&gt;Is this correct?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2015 09:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-ENGcm11135/m-p/409662#M61246</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2015-05-29T09:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 ENGcm11135.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-ENGcm11135/m-p/409663#M61247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;correct!, system should have an active process in secure state, That the reason that init.s includes Write the Cache Size selection register, as published &lt;/P&gt;&lt;P data-canvas-width="289.8424941176471" style="font-size: 16.8235px; font-family: serif;"&gt;sequence for cleaning the entire cache, it save the CSSELR and then restore it value, corresponding to the security state the processor is transitioning.&lt;/P&gt;&lt;P data-canvas-width="289.8424941176471" style="font-size: 16.8235px; font-family: serif;"&gt;Please take in mind that,&amp;nbsp; The specified behavior and that can limit or severely impair the intended use of specified features, but does not render the product unusable in all or the majority of applications&lt;/P&gt;&lt;P data-canvas-width="289.8424941176471" style="font-size: 16.8235px; font-family: serif;"&gt;&lt;/P&gt;&lt;P data-canvas-width="289.8424941176471" style="font-size: 16.8235px; font-family: serif;"&gt;Hope this helps&lt;/P&gt;&lt;P data-canvas-width="289.8424941176471" style="font-size: 16.8235px; font-family: serif;"&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2015 15:10:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-ENGcm11135/m-p/409663#M61247</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2015-06-02T15:10:59Z</dc:date>
    </item>
  </channel>
</rss>