<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMfgTool and USB 3.0</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-and-USB-3-0/m-p/409575#M61216</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two questions related to use the Freescale&amp;nbsp; MfgTool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is MfgTool 2.0 compatible with the .ini and .xml files that are used with MfgTool 1.x?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently using Mfg Tool V1.6.2.048 on Windows 7 and I know it has an issue with USB 3.0. From the following link version V1.6.2.055 fixes this issue. I can't find this on the Freescale website. Is it possible to get a pointer to this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Aug 2015 15:21:53 GMT</pubDate>
    <dc:creator>bdp42</dc:creator>
    <dc:date>2015-08-31T15:21:53Z</dc:date>
    <item>
      <title>MfgTool and USB 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-and-USB-3-0/m-p/409575#M61216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two questions related to use the Freescale&amp;nbsp; MfgTool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is MfgTool 2.0 compatible with the .ini and .xml files that are used with MfgTool 1.x?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently using Mfg Tool V1.6.2.048 on Windows 7 and I know it has an issue with USB 3.0. From the following link version V1.6.2.055 fixes this issue. I can't find this on the Freescale website. Is it possible to get a pointer to this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Aug 2015 15:21:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-and-USB-3-0/m-p/409575#M61216</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2015-08-31T15:21:53Z</dc:date>
    </item>
    <item>
      <title>Re: MfgTool and USB 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-and-USB-3-0/m-p/409576#M61217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Forgot to add link I refer to in the question&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/355524"&gt;https://community.freescale.com/thread/355524&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Aug 2015 15:25:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-and-USB-3-0/m-p/409576#M61217</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2015-08-31T15:25:24Z</dc:date>
    </item>
    <item>
      <title>Re: MfgTool and USB 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-and-USB-3-0/m-p/409577#M61218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bruno&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid that MfgTool 1.x and ver.2.0 are not fully compatible,&lt;/P&gt;&lt;P&gt;so some modification of xml/ini files may be needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Sep 2015 01:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-and-USB-3-0/m-p/409577#M61218</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-01T01:37:39Z</dc:date>
    </item>
    <item>
      <title>Re: MfgTool and USB 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-and-USB-3-0/m-p/409578#M61219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok, Then is it possible to get a pointer to V1.6.2.055 of the Mfg Tool. This may fix the problem I am having.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Sep 2015 08:41:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-and-USB-3-0/m-p/409578#M61219</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2015-09-01T08:41:19Z</dc:date>
    </item>
    <item>
      <title>Re: MfgTool and USB 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-and-USB-3-0/m-p/409579#M61220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did manage to find this version of the MfgTool and it now works on my Windows 7 PC with USB 3.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's the link to the relevant post in case anyone else is looking for it. It's attached as a zip file - mfgtools-rel.7z.zip&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/318706"&gt;https://community.freescale.com/thread/318706&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Sep 2015 09:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-and-USB-3-0/m-p/409579#M61220</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2015-09-01T09:42:23Z</dc:date>
    </item>
  </channel>
</rss>