<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCPU core locked when RTC changed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CPU-core-locked-when-RTC-changed/m-p/409544#M61207</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is a very strange bug. :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We've upgraded from 3.0.35 to 3.14 (on Lollipop 5.1.1-ga) and are experiencing problems with the CPU getting locked up when clock/date is changed. But only one of the cores, and eventually watchdog triggers restart.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This only happens if the unix time set is above 268435456 (0x10000000), setting anything below that works fine.&lt;/P&gt;&lt;P&gt;In other words; the following command works fine.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;EM&gt;date -s 19780704.212400&lt;/EM&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But if running.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;date -s 19780704.212500&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;One of the CPU cores gets locked up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone has any idea what goes wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're running on iMX6DL, and kernel 3.0.35 works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Nov 2015 10:27:01 GMT</pubDate>
    <dc:creator>emilmyhrman</dc:creator>
    <dc:date>2015-11-13T10:27:01Z</dc:date>
    <item>
      <title>CPU core locked when RTC changed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU-core-locked-when-RTC-changed/m-p/409544#M61207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is a very strange bug. :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We've upgraded from 3.0.35 to 3.14 (on Lollipop 5.1.1-ga) and are experiencing problems with the CPU getting locked up when clock/date is changed. But only one of the cores, and eventually watchdog triggers restart.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This only happens if the unix time set is above 268435456 (0x10000000), setting anything below that works fine.&lt;/P&gt;&lt;P&gt;In other words; the following command works fine.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;EM&gt;date -s 19780704.212400&lt;/EM&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But if running.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;date -s 19780704.212500&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;One of the CPU cores gets locked up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone has any idea what goes wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're running on iMX6DL, and kernel 3.0.35 works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Nov 2015 10:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU-core-locked-when-RTC-changed/m-p/409544#M61207</guid>
      <dc:creator>emilmyhrman</dc:creator>
      <dc:date>2015-11-13T10:27:01Z</dc:date>
    </item>
    <item>
      <title>Re: CPU core locked when RTC changed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU-core-locked-when-RTC-changed/m-p/409545#M61208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Fixed! Problem was in our code and differences in 3.0.35 vs 3.14. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Nov 2015 07:54:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU-core-locked-when-RTC-changed/m-p/409545#M61208</guid>
      <dc:creator>emilmyhrman</dc:creator>
      <dc:date>2015-11-17T07:54:43Z</dc:date>
    </item>
  </channel>
</rss>