<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SGTL5000 connection in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-connection/m-p/409173#M61130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Connect the unused Line-In inputs to GND. This is the most effective way to prevent hum/audio noise/RF noise from coupling into the analog circuit. Also, by happy coincidence this is the cheapest way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only "gotcha" - if this is a battery-powered device, just double-check that the codec's idle current is not increased significantly by this connection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Sep 2015 22:20:36 GMT</pubDate>
    <dc:creator>nikolaydimitro1</dc:creator>
    <dc:date>2015-09-24T22:20:36Z</dc:date>
    <item>
      <title>SGTL5000 connection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-connection/m-p/409172#M61129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using a SGTL5000 to play-back audio (using line-out) and capture audio (using mic-input), with an iMX51. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the LINE_IN signals of the SGTL5000 are not used, what is the recommended connection for them? (leave unconnected, tie to GND, tie to GND via a capacitor or resistor...)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The typical application schematic on the datasheet does not clarify what to do with these pins if not used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Sep 2015 16:26:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-connection/m-p/409172#M61129</guid>
      <dc:creator>carlosvernich</dc:creator>
      <dc:date>2015-09-24T16:26:08Z</dc:date>
    </item>
    <item>
      <title>Re: SGTL5000 connection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-connection/m-p/409173#M61130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Connect the unused Line-In inputs to GND. This is the most effective way to prevent hum/audio noise/RF noise from coupling into the analog circuit. Also, by happy coincidence this is the cheapest way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only "gotcha" - if this is a battery-powered device, just double-check that the codec's idle current is not increased significantly by this connection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Sep 2015 22:20:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-connection/m-p/409173#M61130</guid>
      <dc:creator>nikolaydimitro1</dc:creator>
      <dc:date>2015-09-24T22:20:36Z</dc:date>
    </item>
    <item>
      <title>Re: SGTL5000 connection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-connection/m-p/409174#M61131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Nikolay,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That helps me a lot!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Sep 2015 16:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-connection/m-p/409174#M61131</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-09-28T16:53:56Z</dc:date>
    </item>
  </channel>
</rss>