<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6sl compile error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6sl-compile-error/m-p/409099#M61104</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;Thangameena Rajendhiran,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend looking at the RAM usage when compiling. It is recommended to have at least 16GB of RAM or otherwise some errors may occur.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may use a bigger swap in order to increase the “RAM” available. There is some information on the following document:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-102403"&gt;https://community.freescale.com/docs/DOC-102403&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jul 2015 15:55:50 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2015-07-15T15:55:50Z</dc:date>
    <item>
      <title>imx6sl compile error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6sl-compile-error/m-p/409098#M61103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi i am working in imx6sl&amp;nbsp; 4.4.2 kitkat. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while compiling android system.img.&amp;nbsp; using make &lt;/P&gt;&lt;P&gt;i am getting error as&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Install: out/target/product/evk_6sl/system/framework/webviewchromium.odex&lt;/P&gt;&lt;P&gt;target thumb C++: third_party_WebKit_Source_core_webcore_derived_gyp &amp;lt;= external/chromium_org/third_party/WebKit/Source/bindings/v8/custom/V8DocumentCustom.cpp&lt;/P&gt;&lt;P&gt;external/chromium_org/third_party/WebKit/Source/bindings/v8/custom/V8DocumentCustom.cpp:63:86: error: no 'void WebCore::V8Document::evaluateMethodCustom(const v8::FunctionCallbackInfo&amp;lt;v8::Value&amp;gt;&amp;amp;)' member function declared in class 'WebCore::V8Document'&lt;/P&gt;&lt;P&gt;make: *** [out/target/product/evk_6sl/obj/STATIC_LIBRARIES/third_party_WebKit_Source_core_webcore_derived_gyp_intermediates/third_party/WebKit/Source/bindings/v8/custom/V8DocumentCustom.o] Error 1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2015 14:45:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6sl-compile-error/m-p/409098#M61103</guid>
      <dc:creator>thangameenaraje</dc:creator>
      <dc:date>2015-07-14T14:45:17Z</dc:date>
    </item>
    <item>
      <title>Re: imx6sl compile error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6sl-compile-error/m-p/409099#M61104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;Thangameena Rajendhiran,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend looking at the RAM usage when compiling. It is recommended to have at least 16GB of RAM or otherwise some errors may occur.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may use a bigger swap in order to increase the “RAM” available. There is some information on the following document:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-102403"&gt;https://community.freescale.com/docs/DOC-102403&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 15:55:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6sl-compile-error/m-p/409099#M61104</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-07-15T15:55:50Z</dc:date>
    </item>
  </channel>
</rss>