<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Update uImage on iMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Update-uImage-on-iMX6/m-p/409060#M61097</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The fact is that the kernel loaded first time, has no support for cifs, anche the update got it&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, should be ok, add cifs to the actual kernel loaded&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Jun 2015 08:49:07 GMT</pubDate>
    <dc:creator>giorgiofantin</dc:creator>
    <dc:date>2015-06-18T08:49:07Z</dc:date>
    <item>
      <title>Update uImage on iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Update-uImage-on-iMX6/m-p/409059#M61096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&amp;nbsp; i have a big problem (for me),becouse i need to update uImage on my Qt iMX6 while the system is running on MMC. I have a Q7 module, ehere i loaeded u-boot, uImage and FS on the MMC. During the loading, oi copied the wrong uImage and now i have the necessity to update it with the right one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope that someone helps me&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2015 08:00:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Update-uImage-on-iMX6/m-p/409059#M61096</guid>
      <dc:creator>giorgiofantin</dc:creator>
      <dc:date>2015-06-18T08:00:08Z</dc:date>
    </item>
    <item>
      <title>Re: Update uImage on iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Update-uImage-on-iMX6/m-p/409060#M61097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The fact is that the kernel loaded first time, has no support for cifs, anche the update got it&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, should be ok, add cifs to the actual kernel loaded&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2015 08:49:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Update-uImage-on-iMX6/m-p/409060#M61097</guid>
      <dc:creator>giorgiofantin</dc:creator>
      <dc:date>2015-06-18T08:49:07Z</dc:date>
    </item>
    <item>
      <title>Re: Update uImage on iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Update-uImage-on-iMX6/m-p/409061#M61098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To update your image you can try to use mfgtool.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It provides the possibility to update the eMMC with a different image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 13:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Update-uImage-on-iMX6/m-p/409061#M61098</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-06-22T13:44:17Z</dc:date>
    </item>
  </channel>
</rss>