<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUSB mouse plug and play not working</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-mouse-plug-and-play-not-working/m-p/408684#M60981</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using imx 6 Q Sabre SDB board and we are using timestorm linux 3.0.&lt;/P&gt;&lt;P&gt;In our board the USB mouse plug and play functionality not working.&lt;/P&gt;&lt;P&gt;&lt;STRONG style="color: #3d3d3d;"&gt;Scenario 1:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Once board is up,connect USB mouse to the port.&lt;/P&gt;&lt;P&gt;In the terminal it will show &lt;/P&gt;&lt;P&gt;usb 2-1: new low speed USB device number 2 using fsl-ehci&lt;/P&gt;&lt;P&gt;input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input1&lt;/P&gt;&lt;P&gt;generic-usb 0003:0461:4E22.0001: input,hidraw0: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But In the application it is not showing its mouse pointer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Scenario 2 :&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Connect the mouse.Start the board.&lt;/P&gt;&lt;P&gt;We can see mouse pointer in the application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But my question is why mouse pointer is not showing when the board is already up??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Divya R Dharan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jul 2015 09:23:23 GMT</pubDate>
    <dc:creator>divyardharan</dc:creator>
    <dc:date>2015-07-14T09:23:23Z</dc:date>
    <item>
      <title>USB mouse plug and play not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-mouse-plug-and-play-not-working/m-p/408684#M60981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using imx 6 Q Sabre SDB board and we are using timestorm linux 3.0.&lt;/P&gt;&lt;P&gt;In our board the USB mouse plug and play functionality not working.&lt;/P&gt;&lt;P&gt;&lt;STRONG style="color: #3d3d3d;"&gt;Scenario 1:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Once board is up,connect USB mouse to the port.&lt;/P&gt;&lt;P&gt;In the terminal it will show &lt;/P&gt;&lt;P&gt;usb 2-1: new low speed USB device number 2 using fsl-ehci&lt;/P&gt;&lt;P&gt;input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input1&lt;/P&gt;&lt;P&gt;generic-usb 0003:0461:4E22.0001: input,hidraw0: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But In the application it is not showing its mouse pointer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Scenario 2 :&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Connect the mouse.Start the board.&lt;/P&gt;&lt;P&gt;We can see mouse pointer in the application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But my question is why mouse pointer is not showing when the board is already up??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Divya R Dharan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2015 09:23:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-mouse-plug-and-play-not-working/m-p/408684#M60981</guid>
      <dc:creator>divyardharan</dc:creator>
      <dc:date>2015-07-14T09:23:23Z</dc:date>
    </item>
  </channel>
</rss>