<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: iMX28 with mDDR kernel panic</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-mDDR-kernel-panic/m-p/173411#M6058</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vladan,&lt;/P&gt;&lt;P&gt;thanks, but i found what the problems was, i had the "Build mfg firmware" ticked on, this was causing the issue with the boot stream to be overwritten, removing this and rebuilding, setting the boot stream in the kernel configuration and the board is up and running.&lt;/P&gt;&lt;P&gt;Cheers&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Oct 2011 10:47:15 GMT</pubDate>
    <dc:creator>TimWoodham</dc:creator>
    <dc:date>2011-10-04T10:47:15Z</dc:date>
    <item>
      <title>iMX28 with mDDR kernel panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-mDDR-kernel-panic/m-p/173409#M6056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;we've just got back our iMX28 board based on the EVK.&amp;nbsp; The only major difference is that we chose to run mDDR rather than DDR2.&lt;/P&gt;&lt;P&gt;I've built the kernel for mDDR and it mostly runs fine with uBoot etc and memory is being tested and read ok.&lt;/P&gt;&lt;P&gt;The problem i have is that the boot up of the kernel flags this problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;SPAN style="color: #000080;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;mmc0: new high speed SD card at address 0007&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;mmcblk0: mmc0:0007 SU02G 1.83 GiB&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;mmcblk0: p1 p2 p3&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:00:05 UTC (5)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;VFS: Cannot open root device "ubi0:rootfs1" or unknown-block(0,0)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;Please append a correct "root=" boot option; here are the available partitions:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;b300&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1921024 mmcblk0 driver: mmcblk&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;&amp;nbsp; b301&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 35084 mmcblk0p1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;&amp;nbsp; b302&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 35112 mmcblk0p2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;&amp;nbsp; b303&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1849764 mmcblk0p3&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="color: #000080; "&gt;Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;Backtrace:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;[&amp;lt;c00336c4&amp;gt;] (dump_backtrace+0x0/0x114) from [&amp;lt;c03ba940&amp;gt;] (dump_stack+0x18/0x1c)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;r7:c0028a24 r6:00008000 r5:c7c14000 r4:c051b0b8&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;[&amp;lt;c03ba928&amp;gt;] (dump_stack+0x0/0x1c) from [&amp;lt;c03ba9a4&amp;gt;] (panic+0x60/0xdc)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;[&amp;lt;c03ba944&amp;gt;] (panic+0x0/0xdc) from [&amp;lt;c0008fe0&amp;gt;] (mount_block_root+0x1d8/0x218)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;r3:00000000 r2:00000000 r1:c7c27f78 r0:c046a025&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;[&amp;lt;c0008e08&amp;gt;] (mount_block_root+0x0/0x218) from [&amp;lt;c00091b0&amp;gt;] (prepare_namespace+0x94/0x1c4)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;[&amp;lt;c000911c&amp;gt;] (prepare_namespace+0x0/0x1c4) from [&amp;lt;c00084e8&amp;gt;] (kernel_init+0x118/0x158)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;r5:c0027eb8 r4:c051a200&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;[&amp;lt;c00083d0&amp;gt;] (kernel_init+0x0/0x158) from [&amp;lt;c004d1bc&amp;gt;] (do_exit+0x0/0x600)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;r5:c00083d0 r4:00000000]&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; "&gt;After reviewing i can see that the .config file gets changed from&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;CONFIG_PKG_BOOT_STREAM_CMDLINE1="noinitrd console=ttyAM0,115200 root=/dev/mmcblk0p3 rw rootwait ip=none gpmi"&lt;/P&gt;&lt;P&gt;to&lt;/P&gt;&lt;P&gt;CONFIG_PKG_BOOT_STREAM_CMDLINE1="console=ttyAM0,115200 rdinit=/linuxrc rw gpmi"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;after i run the ./ltib -p boot_stream.spec –f&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anyone has got the iMX28 working with mDDR i'd happy to hear how they got on or if they had this problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2011 00:46:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-mDDR-kernel-panic/m-p/173409#M6056</guid>
      <dc:creator>TimWoodham</dc:creator>
      <dc:date>2011-09-28T00:46:47Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 with mDDR kernel panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-mDDR-kernel-panic/m-p/173410#M6057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tim,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;this doesn't have anything to do with mDDR. You just need to adjust the boot parameters that bootstreams will use by default to start the kernel. So:&lt;/P&gt;&lt;P&gt;./ltib --configure&lt;/P&gt;&lt;P&gt;then edit the bootstream parameters&lt;/P&gt;&lt;P&gt;SAVE configuration&lt;/P&gt;&lt;P&gt;once ./ltib is done, rebuild bootstream (won't be done automatically when just bootstream parameters are changed) by:&lt;/P&gt;&lt;P&gt;./ltib -p boot_stream.spec -f&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;br,&lt;/P&gt;&lt;P&gt;Vladan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2011 07:06:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-mDDR-kernel-panic/m-p/173410#M6057</guid>
      <dc:creator>VladanJovanovic</dc:creator>
      <dc:date>2011-09-28T07:06:20Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 with mDDR kernel panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-mDDR-kernel-panic/m-p/173411#M6058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vladan,&lt;/P&gt;&lt;P&gt;thanks, but i found what the problems was, i had the "Build mfg firmware" ticked on, this was causing the issue with the boot stream to be overwritten, removing this and rebuilding, setting the boot stream in the kernel configuration and the board is up and running.&lt;/P&gt;&lt;P&gt;Cheers&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Oct 2011 10:47:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-mDDR-kernel-panic/m-p/173411#M6058</guid>
      <dc:creator>TimWoodham</dc:creator>
      <dc:date>2011-10-04T10:47:15Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 with mDDR kernel panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-mDDR-kernel-panic/m-p/173412#M6059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ok, that makes sense. It looks like too many people tick the "Build mfg firmware" box thinking it will just build one additional package. In reality it affects system configuration a lot and should &lt;STRONG&gt;only&lt;/STRONG&gt; be used on a separate LTIB installation (not the one where you have your development going on) to build a binary used only for updating and nothing else.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Vladan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Oct 2011 05:15:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-mDDR-kernel-panic/m-p/173412#M6059</guid>
      <dc:creator>VladanJovanovic</dc:creator>
      <dc:date>2011-10-05T05:15:41Z</dc:date>
    </item>
  </channel>
</rss>