<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to run Qt5 example application(s) on EPD?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-run-Qt5-example-application-s-on-EPD/m-p/406711#M60550</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Qt required X11 back end and necessary EPD update routines for running the sample applications.&lt;/P&gt;&lt;P&gt;Closing the thread since, I found a workaround to run it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Aug 2015 09:01:14 GMT</pubDate>
    <dc:creator>ajithpv</dc:creator>
    <dc:date>2015-08-11T09:01:14Z</dc:date>
    <item>
      <title>How to run Qt5 example application(s) on EPD?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-run-Qt5-example-application-s-on-EPD/m-p/406709#M60548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;As part of my current task, I'm working on the EPDC of i.MX6 SoloLite. I'm using the Linux kernel version 3.14.28 (Rev. L3.14.28_1.0.0-ga) with Yocto build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I'm running the "./mxc_epdc_fb_test.out" from the board, it is working and showing the test cases one by one. This is confirmed that, the display and basic set-up is working proper.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since, I want to try Qt sample applications (provided in the rootfs) on E-INK EPD, I tried to run it from the board as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN style="text-decoration: underline;"&gt;STEP 1:&lt;/SPAN&gt; Qt applications are running directly from the console&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have run the Qt5 sample applications that are present inside "/usr/share" folder individually. But I'm getting the below error.&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;EM&gt;Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.&lt;/EM&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;EM&gt;Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.&lt;/EM&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;EM&gt;libGL error: dlopen /usr/lib/dri/vivante_dri.so failed (libGL.so.1.2: cannot open shared object file: No such file or directory)&lt;/EM&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;EM&gt;libGL error: unable to load driver: vivante_dri.so&lt;/EM&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;EM&gt;libGL error: failed to load driver: vivante&lt;/EM&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;EM&gt;libpng warning: iCCP: known incorrect sRGB profile&lt;/EM&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;EM&gt;libpng warning: iCCP: known incorrect sRGB profile&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN style="text-decoration: underline;"&gt;STEP 2 :&lt;/SPAN&gt; Running the Qt application through "mxc_epdc_x11_fb_test.out" test application&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have tried to run the test application "mxc_epdc_x11_fb_test.out" under unit_tests folder. This application shows a desktop window with Qt application icons on EPD (display).&lt;/P&gt;&lt;P&gt;When I touch a Qt application icon (via touch panel), then Qt application is working!, without any error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I would like to know what I'm missing. Could anyone please tell me, how I can run the Qt5 application as STEP1 (This is the one I required). How to resolve the above errors?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking forward to your reply...&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;BR /&gt;Ajith P V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2015 09:05:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-run-Qt5-example-application-s-on-EPD/m-p/406709#M60548</guid>
      <dc:creator>ajithpv</dc:creator>
      <dc:date>2015-07-14T09:05:10Z</dc:date>
    </item>
    <item>
      <title>Re: How to run Qt5 example application(s) on EPD?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-run-Qt5-example-application-s-on-EPD/m-p/406710#M60549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Any updates?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2015 06:38:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-run-Qt5-example-application-s-on-EPD/m-p/406710#M60549</guid>
      <dc:creator>ajithpv</dc:creator>
      <dc:date>2015-07-20T06:38:51Z</dc:date>
    </item>
    <item>
      <title>Re: How to run Qt5 example application(s) on EPD?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-run-Qt5-example-application-s-on-EPD/m-p/406711#M60550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Qt required X11 back end and necessary EPD update routines for running the sample applications.&lt;/P&gt;&lt;P&gt;Closing the thread since, I found a workaround to run it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 09:01:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-run-Qt5-example-application-s-on-EPD/m-p/406711#M60550</guid>
      <dc:creator>ajithpv</dc:creator>
      <dc:date>2015-08-11T09:01:14Z</dc:date>
    </item>
  </channel>
</rss>