<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLinux Test Project for i.MX6UL Linux BSP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Test-Project-for-i-MX6UL-Linux-BSP/m-p/406201#M60455</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about LinuxBSP for i.MX6UL.&lt;/P&gt;&lt;P&gt;L3.14.38_iMX6UL (REV L3.14.38_6ul) is released as BSP for i.MX6UL.&lt;/P&gt;&lt;P&gt;Did an LTP test be executed on this BSP?&lt;/P&gt;&lt;P&gt;If there is the result of the LTP test, would you send it to me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Nov 2015 08:02:19 GMT</pubDate>
    <dc:creator>yuuki</dc:creator>
    <dc:date>2015-11-13T08:02:19Z</dc:date>
    <item>
      <title>Linux Test Project for i.MX6UL Linux BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Test-Project-for-i-MX6UL-Linux-BSP/m-p/406201#M60455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about LinuxBSP for i.MX6UL.&lt;/P&gt;&lt;P&gt;L3.14.38_iMX6UL (REV L3.14.38_6ul) is released as BSP for i.MX6UL.&lt;/P&gt;&lt;P&gt;Did an LTP test be executed on this BSP?&lt;/P&gt;&lt;P&gt;If there is the result of the LTP test, would you send it to me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Nov 2015 08:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Test-Project-for-i-MX6UL-Linux-BSP/m-p/406201#M60455</guid>
      <dc:creator>yuuki</dc:creator>
      <dc:date>2015-11-13T08:02:19Z</dc:date>
    </item>
    <item>
      <title>Re: Linux Test Project for i.MX6UL Linux BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Test-Project-for-i-MX6UL-Linux-BSP/m-p/406202#M60456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately ltp-imx package is not supported by Freescale for i.MX6 platform.&lt;/P&gt;&lt;P&gt;Sorry for the inconvenience.&lt;/P&gt;&lt;P&gt;The package ltp-imx was used for early i.MX series, such as i.MX35,51.&lt;/P&gt;&lt;P&gt;Then it was replaced with OBDS - i.MX50,53,28.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Nov 2015 07:54:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Test-Project-for-i-MX6UL-Linux-BSP/m-p/406202#M60456</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2015-11-16T07:54:45Z</dc:date>
    </item>
  </channel>
</rss>