<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックGathering i.MX6 GPIO interrupt</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Gathering-i-MX6-GPIO-interrupt/m-p/405411#M60314</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using i.MX6(SABRE-SDP) and Linux 3.10.53.&lt;/P&gt;&lt;P&gt;There are two buttons labeled Volume Up and Down.&lt;/P&gt;&lt;P&gt;When click those, I got message like below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# dmesg -c&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;[ 2875.895728] evbug: Event. Dev: input1, Type: 1, Code: 114, Value: 0&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;[ 2873.265728] evbug: Event. Dev: input1, Type: 1, Code: 115, Value: 1&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is just kernel messages, I do not know how can handle those interrupt.&lt;/P&gt;&lt;P&gt;So my question is that how can I sense those events in my application?&lt;/P&gt;&lt;P&gt;Is there a linux application guide? For example, when pushing the key, print out debuging message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 May 2015 09:02:55 GMT</pubDate>
    <dc:creator>JHY</dc:creator>
    <dc:date>2015-05-28T09:02:55Z</dc:date>
    <item>
      <title>Gathering i.MX6 GPIO interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gathering-i-MX6-GPIO-interrupt/m-p/405411#M60314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using i.MX6(SABRE-SDP) and Linux 3.10.53.&lt;/P&gt;&lt;P&gt;There are two buttons labeled Volume Up and Down.&lt;/P&gt;&lt;P&gt;When click those, I got message like below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# dmesg -c&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;[ 2875.895728] evbug: Event. Dev: input1, Type: 1, Code: 114, Value: 0&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;[ 2873.265728] evbug: Event. Dev: input1, Type: 1, Code: 115, Value: 1&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is just kernel messages, I do not know how can handle those interrupt.&lt;/P&gt;&lt;P&gt;So my question is that how can I sense those events in my application?&lt;/P&gt;&lt;P&gt;Is there a linux application guide? For example, when pushing the key, print out debuging message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2015 09:02:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gathering-i-MX6-GPIO-interrupt/m-p/405411#M60314</guid>
      <dc:creator>JHY</dc:creator>
      <dc:date>2015-05-28T09:02:55Z</dc:date>
    </item>
    <item>
      <title>Re: Gathering i.MX6 GPIO interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gathering-i-MX6-GPIO-interrupt/m-p/405412#M60315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at linux ../DOC/gpio.txt,input-programming.txt&lt;/P&gt;&lt;P&gt;link below gives useful references&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/310091"&gt;Configure GPIO as interrupt source&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://patchwork.kernel.org/patch/1293451/" rel="nofollow" target="_blank"&gt;https://patchwork.kernel.org/patch/1293451/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2015 11:54:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gathering-i-MX6-GPIO-interrupt/m-p/405412#M60315</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-05-28T11:54:05Z</dc:date>
    </item>
  </channel>
</rss>