<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx287: Using LCDIF as asynchronous memory interface in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx287-Using-LCDIF-as-asynchronous-memory-interface/m-p/404172#M59970</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using a imx287 in a project which requires a high speed interface with a FPGA.&lt;/P&gt;&lt;P&gt;So far we are using a single bit SPI, since our FPGA SPI core doesn't accept dual or quad configurations. Also clock rate is quite limited by the FPGA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And we have found that this channel is a real bottleneck.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To work it out we have been told some time ago that we could use the LCD interface as a bus interface, adding some logic in the FPGA to decode address/data. Being a parellel bus we'll have a real boost that will fit our requirements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are ready to loose our LCD functionality as we are not using it anyway.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone used this LCD interface as asynchronous bus? Default LCD drivers seem quite useless for us. Is there an easy way to get it working?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have searched in the web with no success... Any idea will be welcomed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jul 2015 08:50:55 GMT</pubDate>
    <dc:creator>alexmoreno</dc:creator>
    <dc:date>2015-07-13T08:50:55Z</dc:date>
    <item>
      <title>imx287: Using LCDIF as asynchronous memory interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx287-Using-LCDIF-as-asynchronous-memory-interface/m-p/404172#M59970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using a imx287 in a project which requires a high speed interface with a FPGA.&lt;/P&gt;&lt;P&gt;So far we are using a single bit SPI, since our FPGA SPI core doesn't accept dual or quad configurations. Also clock rate is quite limited by the FPGA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And we have found that this channel is a real bottleneck.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To work it out we have been told some time ago that we could use the LCD interface as a bus interface, adding some logic in the FPGA to decode address/data. Being a parellel bus we'll have a real boost that will fit our requirements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are ready to loose our LCD functionality as we are not using it anyway.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone used this LCD interface as asynchronous bus? Default LCD drivers seem quite useless for us. Is there an easy way to get it working?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have searched in the web with no success... Any idea will be welcomed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2015 08:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx287-Using-LCDIF-as-asynchronous-memory-interface/m-p/404172#M59970</guid>
      <dc:creator>alexmoreno</dc:creator>
      <dc:date>2015-07-13T08:50:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx287: Using LCDIF as asynchronous memory interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx287-Using-LCDIF-as-asynchronous-memory-interface/m-p/404173#M59971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI alex&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of such efforts, but think that one can try&lt;/P&gt;&lt;P&gt;8080 mode driver as starting point&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95559"&gt;Patch for i.MX28's 8080 mode Lcd panel driver&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2015 02:45:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx287-Using-LCDIF-as-asynchronous-memory-interface/m-p/404173#M59971</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-14T02:45:38Z</dc:date>
    </item>
  </channel>
</rss>