<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: No SD Card activity in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/No-SD-Card-activity/m-p/404082#M59920</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi john&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reason that SD card is not booting on new board is that for&lt;/P&gt;&lt;P&gt;new board one needs to run ddr test and rebuild image with new&lt;/P&gt;&lt;P&gt;ddr configuration settings (changing them in uboot dcd header)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V2.20&lt;/A&gt; &lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;more SD interface test can be done with baremetal SDK (drivers/usdhc)&lt;/P&gt;&lt;P&gt;(one can run it with jtag)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94139"&gt;i.MX6 Platform SDK 1.1 Release&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Sep 2015 01:59:06 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-09-24T01:59:06Z</dc:date>
    <item>
      <title>No SD Card activity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-SD-Card-activity/m-p/404081#M59919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a new custom iMx.6 design.&amp;nbsp; I'm able to JTAG using Segger J-Link emulator but when I try to use SD card there is no activity (probing SD clk, cmd, data shows no activity).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is with Boot Mode 10.&amp;nbsp; I can read SRC Boot Mode Register 1 (SRC_SBMR1) via JTAG and the 32-bits boot mode bits are as expected (0x7E3B2940)&lt;/P&gt;&lt;P&gt;I changed Boot Mode to 00 (boot from eFuse).&amp;nbsp; I read the same register again and the bits are as expected, all 0's.&lt;/P&gt;&lt;P&gt;When I use Boot Mode 00 then I observe SD Card (clk, cmd, data), however, Boot Mode 00 is Serial Download.&amp;nbsp; Since Serial Download, it does not load from SD Card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions?&amp;nbsp; Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What else should I look at?&amp;nbsp; My standard approach is Power, Reset, Clock and Boot Settings.&amp;nbsp; As best I can tell, all of them are ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John B.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;UPDATE&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;32-bit boot mode bits were changed from 0x7E3B 2940&amp;nbsp; to 0x7E3B 2840 and now we observe SD card activity.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the iMx6 Dual Lite does not respond to the data.&amp;nbsp; The exact card with standard content boots on the SABRE board.&lt;/P&gt;&lt;P&gt;I see no activity on our Console port (I even probe the rx, tx lines).&amp;nbsp; We're mapped to the same port as the SABRE board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Sep 2015 15:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-SD-Card-activity/m-p/404081#M59919</guid>
      <dc:creator>johnbaczewski</dc:creator>
      <dc:date>2015-09-23T15:26:40Z</dc:date>
    </item>
    <item>
      <title>Re: No SD Card activity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-SD-Card-activity/m-p/404082#M59920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi john&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reason that SD card is not booting on new board is that for&lt;/P&gt;&lt;P&gt;new board one needs to run ddr test and rebuild image with new&lt;/P&gt;&lt;P&gt;ddr configuration settings (changing them in uboot dcd header)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V2.20&lt;/A&gt; &lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;more SD interface test can be done with baremetal SDK (drivers/usdhc)&lt;/P&gt;&lt;P&gt;(one can run it with jtag)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94139"&gt;i.MX6 Platform SDK 1.1 Release&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Sep 2015 01:59:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-SD-Card-activity/m-p/404082#M59920</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-24T01:59:06Z</dc:date>
    </item>
  </channel>
</rss>