<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Issues about DDR Freq</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issues-about-DDR-Freq/m-p/403555#M59807</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; The stress tool suppports several devices of i.MX series. Say, the MMDC &lt;BR /&gt;of i.MX6Q is specified to work up to 528 MHz. But for testing we can apply &lt;/P&gt;&lt;P&gt;more wide frequency area. As for Linux CPUFREQ feature, it provides&lt;/P&gt;&lt;P&gt;optimal working points regarding core and DDR frequencies, but basically&lt;/P&gt;&lt;P&gt;core and DDR frequencies are independent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Aug 2015 05:07:12 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-08-03T05:07:12Z</dc:date>
    <item>
      <title>Issues about DDR Freq</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-about-DDR-Freq/m-p/403552#M59804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, all&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm so confused about some concepts regarding the freq. One is arm core speed,another is DDR freq. And when I run the DDR stress tool, we will see as follow:&lt;/P&gt;&lt;P&gt;And the MMDC support the max freq is 400MHz, Why can we change the freq to more than 400MHz,such as 672MHz? So the freq here means the Arm core speed?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54282i1FEF821C4D06674C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and when I change the governer we will find its max freq(996MHz), its min freq(396MHz), and I think it is arm core speed, So what is the correlation between the freq in governer and in DDR stress tool? Will the DDR freq change when I change the arm core speed via the governer? If so, how can I get the current speed about the DDR? 3Q~&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Aug 2015 02:12:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-about-DDR-Freq/m-p/403552#M59804</guid>
      <dc:creator>tony_l_cai</dc:creator>
      <dc:date>2015-08-03T02:12:57Z</dc:date>
    </item>
    <item>
      <title>Re: Issues about DDR Freq</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-about-DDR-Freq/m-p/403553#M59805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; The DDR stress test is non-OS tool to check how robust DRAM interface is, &lt;/P&gt;&lt;P&gt;given current set of parameters (i.e. drive strength settings, timing parameters, &lt;/P&gt;&lt;P&gt;board layout, etc), therefore it implements testing even out of the specified&lt;/P&gt;&lt;P&gt;operation range. The test allows to provide checking for DDR frequencies&lt;/P&gt;&lt;P&gt;from 135 till 672 MHz. &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Aug 2015 02:41:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-about-DDR-Freq/m-p/403553#M59805</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-03T02:41:53Z</dc:date>
    </item>
    <item>
      <title>Re: Issues about DDR Freq</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-about-DDR-Freq/m-p/403554#M59806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，Yuri&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; you mean that MMDC can support 400MHz, but we can test the freq from 135MHz to 672MHz? And I need to know whether the DDR freq can change after the governor freq(the ARM core speed freq) changing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Aug 2015 02:55:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-about-DDR-Freq/m-p/403554#M59806</guid>
      <dc:creator>tony_l_cai</dc:creator>
      <dc:date>2015-08-03T02:55:38Z</dc:date>
    </item>
    <item>
      <title>Re: Issues about DDR Freq</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-about-DDR-Freq/m-p/403555#M59807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; The stress tool suppports several devices of i.MX series. Say, the MMDC &lt;BR /&gt;of i.MX6Q is specified to work up to 528 MHz. But for testing we can apply &lt;/P&gt;&lt;P&gt;more wide frequency area. As for Linux CPUFREQ feature, it provides&lt;/P&gt;&lt;P&gt;optimal working points regarding core and DDR frequencies, but basically&lt;/P&gt;&lt;P&gt;core and DDR frequencies are independent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Aug 2015 05:07:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-about-DDR-Freq/m-p/403555#M59807</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-03T05:07:12Z</dc:date>
    </item>
  </channel>
</rss>