<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to use &amp;quot;pcie EC and RC verify system&amp;quot;? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-quot-pcie-EC-and-RC-verify-system-quot/m-p/403355#M59746</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;dear sir:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have readed this link &lt;/SPAN&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="95014" data-objecttype="102" href="https://community.freescale.com/docs/DOC-95014"&gt;https://community.freescale.com/docs/DOC-95014&lt;/A&gt;&lt;/P&gt;&lt;P&gt;fsl's link description as blow:&lt;/P&gt;&lt;P&gt;Connected by 2*mini_PCIe to standard_PCIe&amp;nbsp; adaptors, 2*PEX cable adaptors,&amp;nbsp; and one PCIe cable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my question is:&lt;/P&gt;&lt;P&gt;1,"mini_PCIe to standard_PCIe&amp;nbsp; adaptors" is&amp;nbsp; what? where can I got it?&lt;/P&gt;&lt;P&gt;2,"PEX cable adaptors" is what? where can I got it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 01 Aug 2015 12:40:35 GMT</pubDate>
    <dc:creator>mingmingyuan</dc:creator>
    <dc:date>2015-08-01T12:40:35Z</dc:date>
    <item>
      <title>How to use "pcie EC and RC verify system"?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-quot-pcie-EC-and-RC-verify-system-quot/m-p/403354#M59745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;dear freescal:&lt;/P&gt;&lt;P&gt;I want to verify my pcie bus, but I don't know how to connect two board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Aug 2015 12:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-quot-pcie-EC-and-RC-verify-system-quot/m-p/403354#M59745</guid>
      <dc:creator>mingmingyuan</dc:creator>
      <dc:date>2015-08-01T12:31:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to use "pcie EC and RC verify system"?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-quot-pcie-EC-and-RC-verify-system-quot/m-p/403355#M59746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;dear sir:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have readed this link &lt;/SPAN&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="95014" data-objecttype="102" href="https://community.freescale.com/docs/DOC-95014"&gt;https://community.freescale.com/docs/DOC-95014&lt;/A&gt;&lt;/P&gt;&lt;P&gt;fsl's link description as blow:&lt;/P&gt;&lt;P&gt;Connected by 2*mini_PCIe to standard_PCIe&amp;nbsp; adaptors, 2*PEX cable adaptors,&amp;nbsp; and one PCIe cable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my question is:&lt;/P&gt;&lt;P&gt;1,"mini_PCIe to standard_PCIe&amp;nbsp; adaptors" is&amp;nbsp; what? where can I got it?&lt;/P&gt;&lt;P&gt;2,"PEX cable adaptors" is what? where can I got it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Aug 2015 12:40:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-quot-pcie-EC-and-RC-verify-system-quot/m-p/403355#M59746</guid>
      <dc:creator>mingmingyuan</dc:creator>
      <dc:date>2015-08-01T12:40:35Z</dc:date>
    </item>
    <item>
      <title>Re: How to use "pcie EC and RC verify system"?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-quot-pcie-EC-and-RC-verify-system-quot/m-p/403356#M59747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI mingmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you should by these two cards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.bplus.com.tw/Adapter/PM2C.html" title="http://www.bplus.com.tw/Adapter/PM2C.html"&gt;PM2C V2.1 (PCI-E / Mini PCI-E adapter)&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then manually solder sata cable between them&lt;/P&gt;&lt;P&gt;please read carefully 'How to make it"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95014"&gt;i.MX6Q PCIe EP/RC Validation System&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Aug 2015 15:27:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-quot-pcie-EC-and-RC-verify-system-quot/m-p/403356#M59747</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-08-01T15:27:05Z</dc:date>
    </item>
    <item>
      <title>Re: How to use "pcie EC and RC verify system"?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-quot-pcie-EC-and-RC-verify-system-quot/m-p/403357#M59748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;dear sir：&lt;/P&gt;&lt;P&gt;I have build image and flash image to EP board and RC board.&lt;/P&gt;&lt;P&gt;when system boot, I also look the log as below, so I think pcie link is OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but when I test send and receive data, result is fail. can you help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my test cmd:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EP side:&lt;/P&gt;&lt;P&gt;root@freescale /unit_tests$ ./memtool&amp;nbsp; -32 01000000=deadbeaf&lt;/P&gt;&lt;P&gt;Writing 32-bit value 0xDEADBEAF to address 0x01000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RC side:&lt;/P&gt;&lt;P&gt;root@freescale /unit_tests$ ./memtool&amp;nbsp; -32 40000000 10&lt;/P&gt;&lt;P&gt;E&lt;/P&gt;&lt;P&gt;Reading 0x10 count starting at address 0x40000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x40000000:&amp;nbsp; DFFBFF4B DFFE3E75 7FF8FBFF 7FDBFEDD&lt;/P&gt;&lt;P&gt;0x40000010:&amp;nbsp; FEDA7DFA 7FFF58FF FF2DFEDA 5FDD3CFD&lt;/P&gt;&lt;P&gt;0x40000020:&amp;nbsp; F9F0FCBF 7FADADE7 EFF7FDEC FF797FED&lt;/P&gt;&lt;P&gt;0x40000030:&amp;nbsp; FDF3FFFD 7E8DEDEF FB077D2D BFFDF8FD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;boot log:&lt;/P&gt;&lt;P&gt;iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.&lt;/P&gt;&lt;P&gt;PCIE: imx_pcie_pltfm_probe start link up.&lt;/P&gt;&lt;P&gt;IMX PCIe port: link up.&lt;/P&gt;&lt;P&gt;PCI: bus0: Fast back to back transfers disabled&lt;/P&gt;&lt;P&gt;PCI: bus1: Fast back to back transfers enabled&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff 64bit pref]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: set to [mem 0x01000000-0x010fffff 64bit pref] (PCI address [0x1000000-0x10fffff])&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PCI bridge to [bus 01-01]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0:&amp;nbsp;&amp;nbsp; bridge window [io&amp;nbsp; disabled]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0:&amp;nbsp;&amp;nbsp; bridge window [mem disabled]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0:&amp;nbsp;&amp;nbsp; bridge window [mem pref disabled]&lt;/P&gt;&lt;P&gt;PCI: enabling device 0000:00:00.0 (0000 -&amp;gt; 0003)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Aug 2015 13:25:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-quot-pcie-EC-and-RC-verify-system-quot/m-p/403357#M59748</guid>
      <dc:creator>mingmingyuan</dc:creator>
      <dc:date>2015-08-16T13:25:53Z</dc:date>
    </item>
  </channel>
</rss>