<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: The USB OTG  Sabre board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/The-USB-OTG-Sabre-board/m-p/403292#M59737</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pat,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could also use the native USB Host port that is available at the PCI port. You would need a PCI to USB adapter like:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.amazon.com/SOOGOOD-PCI-E-Adapter-MiniCard-USB2-0/dp/B00JPY5V38/ref=sr_1_1?ie=UTF8&amp;amp;qid=1421278010&amp;amp;sr=8-1&amp;amp;keywords=mini+pcie+half+card+to+usb+2.0+adapter" title="http://www.amazon.com/SOOGOOD-PCI-E-Adapter-MiniCard-USB2-0/dp/B00JPY5V38/ref=sr_1_1?ie=UTF8&amp;amp;qid=1421278010&amp;amp;sr=8-1&amp;amp;keywords=mini+pcie+half+card+to+usb+2.0+adapter"&gt;http://www.amazon.com/SOOGOOD-PCI-E-Adapter-MiniCard-USB2-0/dp/B00JPY5V38/ref=sr_1_1?ie=UTF8&amp;amp;qid=1421278010&amp;amp;sr=8-1&amp;amp;keywords=mini+pcie+half+card+to+usb+2.0+adapter&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tested it (under Linux) on a imx6q-sabresd and it worked fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Apr 2015 03:04:56 GMT</pubDate>
    <dc:creator>fabio_estevam</dc:creator>
    <dc:date>2015-04-14T03:04:56Z</dc:date>
    <item>
      <title>The USB OTG  Sabre board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-USB-OTG-Sabre-board/m-p/403290#M59735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, can I have help with this question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using WIndows OS using an i.MX6 Sabre Board:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB OTG board is the only USB port exposed by the Sabre board so we had to use it when connecting a USB stick with the Windows image. &lt;/P&gt;&lt;P&gt;Since it is an OTG code, we had to configure it by the UEFI software to ‘host mode’.&lt;/P&gt;&lt;P&gt;My question is, is there a way to lock the OTG port to ‘host mode’? Locking means, configuring it so ‘reset port’ does not revert it back to ‘idle’.&lt;/P&gt;&lt;P&gt;I have noticed that GPIO_1 can be configured as USB_OTG_ID. Does that have any effect on the USB OTG&amp;nbsp; port configuration, or can it be used for the “locking” the ‘host mode’ configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Pat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Apr 2015 21:52:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-USB-OTG-Sabre-board/m-p/403290#M59735</guid>
      <dc:creator>PatrickStilwell</dc:creator>
      <dc:date>2015-04-13T21:52:16Z</dc:date>
    </item>
    <item>
      <title>Re: The USB OTG  Sabre board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-USB-OTG-Sabre-board/m-p/403291#M59736</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Patrick&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is not possible to “lock” USB OTG to ‘host mode’ configuration,&lt;/P&gt;&lt;P&gt;USB_OTG_ID can not be used for this.&lt;/P&gt;&lt;P&gt;USB OTG can be programmed in software to support only host mode,&lt;/P&gt;&lt;P&gt;also USB_OTG_ID is processed in software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2015 01:40:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-USB-OTG-Sabre-board/m-p/403291#M59736</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-14T01:40:34Z</dc:date>
    </item>
    <item>
      <title>Re: The USB OTG  Sabre board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-USB-OTG-Sabre-board/m-p/403292#M59737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pat,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could also use the native USB Host port that is available at the PCI port. You would need a PCI to USB adapter like:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.amazon.com/SOOGOOD-PCI-E-Adapter-MiniCard-USB2-0/dp/B00JPY5V38/ref=sr_1_1?ie=UTF8&amp;amp;qid=1421278010&amp;amp;sr=8-1&amp;amp;keywords=mini+pcie+half+card+to+usb+2.0+adapter" title="http://www.amazon.com/SOOGOOD-PCI-E-Adapter-MiniCard-USB2-0/dp/B00JPY5V38/ref=sr_1_1?ie=UTF8&amp;amp;qid=1421278010&amp;amp;sr=8-1&amp;amp;keywords=mini+pcie+half+card+to+usb+2.0+adapter"&gt;http://www.amazon.com/SOOGOOD-PCI-E-Adapter-MiniCard-USB2-0/dp/B00JPY5V38/ref=sr_1_1?ie=UTF8&amp;amp;qid=1421278010&amp;amp;sr=8-1&amp;amp;keywords=mini+pcie+half+card+to+usb+2.0+adapter&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tested it (under Linux) on a imx6q-sabresd and it worked fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2015 03:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-USB-OTG-Sabre-board/m-p/403292#M59737</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2015-04-14T03:04:56Z</dc:date>
    </item>
    <item>
      <title>Re: The USB OTG  Sabre board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-USB-OTG-Sabre-board/m-p/403293#M59738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If OS analyzes&amp;nbsp; the USB_OTG_ID signals in order to select USB mode, one can pull down&lt;BR /&gt;the USB_OTG_ID in order to force OS entering USB host mode.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2015 06:18:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-USB-OTG-Sabre-board/m-p/403293#M59738</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-04-14T06:18:25Z</dc:date>
    </item>
  </channel>
</rss>