<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックchanging U-boot environment variables for HDMI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/changing-U-boot-environment-variables-for-HDMI/m-p/403288#M59733</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are working on i.mx6 custom designed board. We have power it up for the first time and want port OS to the board. We are working on a host system with Ubuntu 14.04 and i.mx6 board is connected to host system through USB. We are bringing up the board (Os porting) by using Yocto training material as given below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="94849" data-objecttype="102" href="https://community.nxp.com/docs/DOC-94849"&gt;Yocto Training - HOME&lt;/A&gt; (&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="94849" data-objecttype="102" href="https://community.nxp.com/docs/DOC-94849"&gt;https://community.freescale.com/docs/DOC-94849&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In conf/local.conf file,I have stated my machine as sabresd and run all commands as per the training document. and deployed sdcard image to sd card. When iam booting the board with the sd card connected, then display is not coming (which is conncted through HDMI cable).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in task #4 , we are doing the following steps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H3&gt;Deploy&lt;/H3&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Deploy the &lt;STRONG&gt;sdcard&lt;/STRONG&gt; image:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;$ sudo dd if=fsl-image-gui-imx6qsabresd.sdcard of=/dev/sdX bs=1M&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or, deploy the &lt;STRONG&gt;ext3&lt;/STRONG&gt; rootfs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;$ sudo dd if=fsl-image-gui-imx6qsabresd.ext3 of=/dev/sdX2 bs=1M&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or deploy only the &lt;STRONG&gt;tar.bz&lt;/STRONG&gt; rootfs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;$ sudo mount /dev/sdX2 /mnt/card&lt;/P&gt;&lt;P&gt;$ sudo tar xf imagename-imx53qsb.tar.bz2 -C /mnt/card&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to deploy only &lt;STRONG&gt;kernel&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;$ sudo cp uImage-3.0.35-r32.10-imx6qsabresd-20130505174618.bin /media/Boot&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to&amp;nbsp; deploy only &lt;STRONG&gt;u-boot&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;$ sudo dd if=u-boot-imx6qsabresd-v2012.10-r3.imx of=/dev/sdX bs=512 seek=2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have deployed sdcard image.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If using HDMI please, modify u-boot environment arguments:&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;STRONG&gt;setenv mmcargs "setenv bootargs console=${console},${baudrate} root=${mmcroot} rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24"&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;how can i set environment variables in u-boot. which file i should work on and do i need to use some tools to set environment variables in u-boot???&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class="js-outcome-helpful-counts-container j-outcome-helpful-counts-container font-color-okay" data-display-overall="true" data-helpful-count="0" data-object-id="526451" data-object-type="2" data-overall-count="0"&gt;&lt;/SPAN&gt;&lt;SPAN class="j-liking-control js-liking-control"&gt;&lt;SPAN class="acclaim-container"&gt;&lt;SPAN class="js-acclaim-container acclaim-like-container" data-acclaim-count="0" data-can-apply="false" data-show-icon="false" data-type="mini"&gt;&lt;SPAN class="j-social-action"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jun 2015 12:12:15 GMT</pubDate>
    <dc:creator>srinivasaporam</dc:creator>
    <dc:date>2015-06-16T12:12:15Z</dc:date>
    <item>
      <title>changing U-boot environment variables for HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/changing-U-boot-environment-variables-for-HDMI/m-p/403288#M59733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are working on i.mx6 custom designed board. We have power it up for the first time and want port OS to the board. We are working on a host system with Ubuntu 14.04 and i.mx6 board is connected to host system through USB. We are bringing up the board (Os porting) by using Yocto training material as given below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="94849" data-objecttype="102" href="https://community.nxp.com/docs/DOC-94849"&gt;Yocto Training - HOME&lt;/A&gt; (&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="94849" data-objecttype="102" href="https://community.nxp.com/docs/DOC-94849"&gt;https://community.freescale.com/docs/DOC-94849&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In conf/local.conf file,I have stated my machine as sabresd and run all commands as per the training document. and deployed sdcard image to sd card. When iam booting the board with the sd card connected, then display is not coming (which is conncted through HDMI cable).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in task #4 , we are doing the following steps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H3&gt;Deploy&lt;/H3&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Deploy the &lt;STRONG&gt;sdcard&lt;/STRONG&gt; image:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;$ sudo dd if=fsl-image-gui-imx6qsabresd.sdcard of=/dev/sdX bs=1M&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or, deploy the &lt;STRONG&gt;ext3&lt;/STRONG&gt; rootfs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;$ sudo dd if=fsl-image-gui-imx6qsabresd.ext3 of=/dev/sdX2 bs=1M&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or deploy only the &lt;STRONG&gt;tar.bz&lt;/STRONG&gt; rootfs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;$ sudo mount /dev/sdX2 /mnt/card&lt;/P&gt;&lt;P&gt;$ sudo tar xf imagename-imx53qsb.tar.bz2 -C /mnt/card&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to deploy only &lt;STRONG&gt;kernel&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;$ sudo cp uImage-3.0.35-r32.10-imx6qsabresd-20130505174618.bin /media/Boot&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to&amp;nbsp; deploy only &lt;STRONG&gt;u-boot&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;$ sudo dd if=u-boot-imx6qsabresd-v2012.10-r3.imx of=/dev/sdX bs=512 seek=2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have deployed sdcard image.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If using HDMI please, modify u-boot environment arguments:&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;STRONG&gt;setenv mmcargs "setenv bootargs console=${console},${baudrate} root=${mmcroot} rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24"&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;how can i set environment variables in u-boot. which file i should work on and do i need to use some tools to set environment variables in u-boot???&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class="js-outcome-helpful-counts-container j-outcome-helpful-counts-container font-color-okay" data-display-overall="true" data-helpful-count="0" data-object-id="526451" data-object-type="2" data-overall-count="0"&gt;&lt;/SPAN&gt;&lt;SPAN class="j-liking-control js-liking-control"&gt;&lt;SPAN class="acclaim-container"&gt;&lt;SPAN class="js-acclaim-container acclaim-like-container" data-acclaim-count="0" data-can-apply="false" data-show-icon="false" data-type="mini"&gt;&lt;SPAN class="j-social-action"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2015 12:12:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/changing-U-boot-environment-variables-for-HDMI/m-p/403288#M59733</guid>
      <dc:creator>srinivasaporam</dc:creator>
      <dc:date>2015-06-16T12:12:15Z</dc:date>
    </item>
    <item>
      <title>Re: changing U-boot environment variables for HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/changing-U-boot-environment-variables-for-HDMI/m-p/403289#M59734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Srinivasa&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reason for display is not coming, may be:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bug 6703 - Kernel hangs on boot when HDMI cable is plugged &lt;/P&gt;&lt;P&gt;&lt;A href="https://bugzilla.yoctoproject.org/show_bug.cgi?id=6703" title="https://bugzilla.yoctoproject.org/show_bug.cgi?id=6703"&gt;https://bugzilla.yoctoproject.org/show_bug.cgi?id=6703&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also one can refer to short tutorial&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95017"&gt;Linux on the i.MX6 sabre sd platform in a few commands&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;for setting environment variables in u-boot one can look&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;A href="http://www.denx.de/wiki/U-Boot" title="http://www.denx.de/wiki/U-Boot"&gt;WebHome &amp;lt; U-Boot &amp;lt; DENX&lt;/A&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2015 01:19:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/changing-U-boot-environment-variables-for-HDMI/m-p/403289#M59734</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-17T01:19:34Z</dc:date>
    </item>
  </channel>
</rss>