<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Intermittent U-Boot USB Mass Storage issues with mx6sxsabresd</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403070#M59718</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I guess that I'm experiencing the same issue and therefore started this discussion on the u-boot mailing list: &lt;A href="http://lists.denx.de/pipermail/u-boot/2016-February/244464.html" title="http://lists.denx.de/pipermail/u-boot/2016-February/244464.html"&gt;[U-Boot] Issue with USB mass storage (thumb drives)&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Feb 2016 10:43:15 GMT</pubDate>
    <dc:creator>friederschrempf</dc:creator>
    <dc:date>2016-02-03T10:43:15Z</dc:date>
    <item>
      <title>Intermittent U-Boot USB Mass Storage issues with mx6sxsabresd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403063#M59711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm in the process of implementing a simple u-boot based upgrade system, and have encountered some issues with large file transfers on certain USB sticks. I've seen the issue on both u-boot-imx v2015.04 and with u-boot-fslc v2015.10.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;U-Boot 2015.10-rc4+fslc+g1fb68c8 (Oct 15 2015 - 12:45:53 -0400)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6SX rev1.2 996 MHz (running at 792 MHz)&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Extended Commercial temperature grade (-20C to 105C) at 52C&lt;/P&gt;&lt;P&gt;Reset cause: WDOG&lt;/P&gt;&lt;P&gt;Board: MX6SX SABRE SDB&lt;/P&gt;&lt;P&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 1 GiB&lt;/P&gt;&lt;P&gt;PMIC:&amp;nbsp; PFUZE100 ID=0x11&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;/P&gt;&lt;P&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PCI:&amp;nbsp;&amp;nbsp; pcie phy link never came up&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Net:&amp;nbsp;&amp;nbsp; Phy 1 not found&lt;/P&gt;&lt;P&gt;FEC [PRIME]&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;/P&gt;&lt;P&gt;=&amp;gt; usb start&lt;/P&gt;&lt;P&gt;starting USB...&lt;/P&gt;&lt;P&gt;USB0:&amp;nbsp;&amp;nbsp; USB EHCI 1.00&lt;/P&gt;&lt;P&gt;scanning bus 0 for devices... 2 USB Device(s) found&lt;/P&gt;&lt;P&gt;USB1:&amp;nbsp;&amp;nbsp; USB EHCI 1.00&lt;/P&gt;&lt;P&gt;scanning bus 1 for devices... 1 USB Device(s) found&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scanning usb for storage devices... 1 Storage Device(s) found&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scanning usb for ethernet devices... 0 Ethernet Device(s) found&lt;/P&gt;&lt;P&gt;=&amp;gt; load usb 0:1 ${loadaddr} rootfs-a.ext4&lt;/P&gt;&lt;P&gt;reading rootfs-a.ext4&lt;/P&gt;&lt;P&gt;EHCI timed out on TD - token=0x1e008d80&lt;/P&gt;&lt;P&gt;EHCI timed out on TD - token=0x9e008d80&lt;/P&gt;&lt;P&gt;EHCI timed out on TD - token=0x800d8d80&lt;/P&gt;&lt;P&gt;EHCI timed out on TD - token=0x1e008d80&lt;/P&gt;&lt;P&gt;Error reading cluster&lt;/P&gt;&lt;P&gt;** Unable to read file rootfs-a.ext4 **&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue comes and goes with no pattern I've been able to discern, but is more reproducible with some USB drives than others. The rootfs-a file is ~400MiB, and the first "time out" errors occur within ~5 seconds of running the "load" command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can reproduce the issue either on the host USB port or the OTG port with the correct cable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've had no issues with a separate 8MiB file even on the most problematic of drives.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have any suggestions for this? I did some fairly thorough searching and was able to find other people with the same problem, but no solutions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Oct 2015 20:03:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403063#M59711</guid>
      <dc:creator>mitchelljohnson</dc:creator>
      <dc:date>2015-10-15T20:03:41Z</dc:date>
    </item>
    <item>
      <title>Re: Intermittent U-Boot USB Mass Storage issues with mx6sxsabresd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403064#M59712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mitchel,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif;"&gt;Your issue is being internally discussed with AE team. As soon as getting news, I will send you an update here. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif;"&gt;Hope this will be useful for you. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif;"&gt;Best regards! &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif;"&gt;/Carlos&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Oct 2015 01:26:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403064#M59712</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-10-23T01:26:24Z</dc:date>
    </item>
    <item>
      <title>Re: Intermittent U-Boot USB Mass Storage issues with mx6sxsabresd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403065#M59713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mitchel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the loadaddr? I see this command&lt;/P&gt;&lt;P&gt; &lt;STRONG&gt;load usb 0:1 ${loadaddr} rootfs-a.ext4&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Often if the address is wrong you will get the timeout errors. Try a fatload from mmc card first to see if the address is correct.&amp;nbsp; If it still fails please printenv and post the contents of the u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2015 23:02:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403065#M59713</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-10-29T23:02:43Z</dc:date>
    </item>
    <item>
      <title>Re: Intermittent U-Boot USB Mass Storage issues with mx6sxsabresd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403066#M59714</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to load the same rootfs from an SD card partition just fine.&lt;/P&gt;&lt;P&gt;=&amp;gt; load mmc 2:4 ${loadaddr} rootfs-a.ext4&lt;/P&gt;&lt;P&gt;406847488 bytes read in 19261 ms (20.1 MiB/s)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I had mentioned before, this seems to be an issue with varying USB sticks. Some work, some do not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are the contents of an env print, as well as the output of bdinfo.&lt;/P&gt;&lt;P&gt;=&amp;gt; env print&lt;/P&gt;&lt;P&gt;baudrate=115200&lt;/P&gt;&lt;P&gt;boot_fdt=try&lt;/P&gt;&lt;P&gt;bootcmd=mmc dev ${mmcdev};mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi&lt;/P&gt;&lt;P&gt;bootdelay=3&lt;/P&gt;&lt;P&gt;bootscript=echo Running bootscript from mmc ...; source&lt;/P&gt;&lt;P&gt;console=ttymxc0&lt;/P&gt;&lt;P&gt;ethact=FEC&lt;/P&gt;&lt;P&gt;ethaddr=00:04:9f:03:85:a4&lt;/P&gt;&lt;P&gt;ethprime=FEC&lt;/P&gt;&lt;P&gt;fdt_addr=0x88000000&lt;/P&gt;&lt;P&gt;fdt_file=imx6sx-sharp-lcd.dtb&lt;/P&gt;&lt;P&gt;fdt_high=0xffffffff&lt;/P&gt;&lt;P&gt;filesize=18400000&lt;/P&gt;&lt;P&gt;image=zImage&lt;/P&gt;&lt;P&gt;initrd_high=0xffffffff&lt;/P&gt;&lt;P&gt;ip_dyn=yes&lt;/P&gt;&lt;P&gt;loadaddr=0x82000000&lt;/P&gt;&lt;P&gt;loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};&lt;/P&gt;&lt;P&gt;loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}&lt;/P&gt;&lt;P&gt;loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}&lt;/P&gt;&lt;P&gt;mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot} fbcon=rotate:1 vt.global_cursor_default=0&lt;/P&gt;&lt;P&gt;mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;&lt;/P&gt;&lt;P&gt;mmcdev=2&lt;/P&gt;&lt;P&gt;mmcpart=1&lt;/P&gt;&lt;P&gt;mmcroot=/dev/mmcblk3p2 rootwait rw&lt;/P&gt;&lt;P&gt;netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp&lt;/P&gt;&lt;P&gt;netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;&lt;/P&gt;&lt;P&gt;script=boot.scr&lt;/P&gt;&lt;P&gt;stderr=serial&lt;/P&gt;&lt;P&gt;stdin=serial&lt;/P&gt;&lt;P&gt;stdout=serial&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Environment size: 1770/8188 bytes&lt;/P&gt;&lt;P&gt;=&amp;gt; bdinfo&lt;/P&gt;&lt;P&gt;arch_number = 0x00000000&lt;/P&gt;&lt;P&gt;boot_params = 0x80000100&lt;/P&gt;&lt;P&gt;DRAM bank&amp;nbsp;&amp;nbsp; = 0x00000000&lt;/P&gt;&lt;P&gt;-&amp;gt; start&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0x80000000&lt;/P&gt;&lt;P&gt;-&amp;gt; size&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0x40000000&lt;/P&gt;&lt;P&gt;eth0name&amp;nbsp;&amp;nbsp;&amp;nbsp; = FEC&lt;/P&gt;&lt;P&gt;ethaddr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 00:04:9f:03:85:a4&lt;/P&gt;&lt;P&gt;current eth = FEC&lt;/P&gt;&lt;P&gt;ip_addr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = &amp;lt;NULL&amp;gt;&lt;/P&gt;&lt;P&gt;baudrate&amp;nbsp;&amp;nbsp;&amp;nbsp; = 115200 bps&lt;/P&gt;&lt;P&gt;TLB addr&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0xBFFF0000&lt;/P&gt;&lt;P&gt;relocaddr&amp;nbsp;&amp;nbsp; = 0xBFF57000&lt;/P&gt;&lt;P&gt;reloc off&amp;nbsp;&amp;nbsp; = 0x38757000&lt;/P&gt;&lt;P&gt;irq_sp&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0xBFC54EA0&lt;/P&gt;&lt;P&gt;sp start&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0xBFC54E90&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Oct 2015 14:27:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403066#M59714</guid>
      <dc:creator>mitchelljohnson</dc:creator>
      <dc:date>2015-10-30T14:27:50Z</dc:date>
    </item>
    <item>
      <title>Re: Intermittent U-Boot USB Mass Storage issues with mx6sxsabresd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403067#M59715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MItchell,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please report this issue in the U-boot mailing list: &lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:u-boot@lists.denx.de"&gt;u-boot@lists.denx.de&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Oct 2015 17:27:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403067#M59715</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2015-10-30T17:27:09Z</dc:date>
    </item>
    <item>
      <title>Re: Intermittent U-Boot USB Mass Storage issues with mx6sxsabresd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403068#M59716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mitchell,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you change the loadaddr to 0x80800000 and give it a try? On my solox board, I got the same errors with the load address you're using but the errors have disappeared with 0x80800000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;EDIT&lt;/STRONG&gt;: Nevermind - I had stopped usb prior to using 0x82000000 but forgotten to restart it afterwards and u-boot didn't pick that up. 0x82000000 seems fine for me now with 3 different USB sticks and 425M file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In that case I suggest changing this macro in include/usb.h and see if the timeouts disappear:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define USB_TIMEOUT_MS(pipe) (usb_pipebulk(pipe) ? 5000 : 1000)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd recommend something like 30000 : 10000 for testing for the time being.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Nov 2015 17:25:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403068#M59716</guid>
      <dc:creator>KursadOney</dc:creator>
      <dc:date>2015-11-09T17:25:27Z</dc:date>
    </item>
    <item>
      <title>Re: Intermittent U-Boot USB Mass Storage issues with mx6sxsabresd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403069#M59717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mitchel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;AE team mentioned that it seems that there is some lack of compatibility (maybe with geometry) of the USB flash drive(s). If you can find a particular brand or size that fails consistently, then they can create a ticket to address it.&lt;/P&gt;&lt;P&gt;Is there a common difference? Is the failing drive 4 GB, 32 GB, or larger? How is it formatted? FAT, VFAT, EXT3, EXT4?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Nov 2015 23:49:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403069#M59717</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-11-09T23:49:12Z</dc:date>
    </item>
    <item>
      <title>Re: Intermittent U-Boot USB Mass Storage issues with mx6sxsabresd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403070#M59718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I guess that I'm experiencing the same issue and therefore started this discussion on the u-boot mailing list: &lt;A href="http://lists.denx.de/pipermail/u-boot/2016-February/244464.html" title="http://lists.denx.de/pipermail/u-boot/2016-February/244464.html"&gt;[U-Boot] Issue with USB mass storage (thumb drives)&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Feb 2016 10:43:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403070#M59718</guid>
      <dc:creator>friederschrempf</dc:creator>
      <dc:date>2016-02-03T10:43:15Z</dc:date>
    </item>
    <item>
      <title>Re: Intermittent U-Boot USB Mass Storage issues with mx6sxsabresd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403071#M59719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just for those who need a quick workaround: Reducing the value of USB_MAX_XFER_BLK in &lt;EM&gt;common/usb_storage.c &lt;/EM&gt;should do the trick (thanks to Sergei Temerkhanov for the hint).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The U-Boot guys are currently working on a solution...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2016 09:56:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Intermittent-U-Boot-USB-Mass-Storage-issues-with-mx6sxsabresd/m-p/403071#M59719</guid>
      <dc:creator>friederschrempf</dc:creator>
      <dc:date>2016-06-02T09:56:32Z</dc:date>
    </item>
  </channel>
</rss>