<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB support at u-boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402910#M59683</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fabio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My intention is to boot the kernel and filesystem from u-boot prompt through USB. The board already has u-boot in eMMC. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Sep 2015 06:16:26 GMT</pubDate>
    <dc:creator>manjunathjoshi</dc:creator>
    <dc:date>2015-09-25T06:16:26Z</dc:date>
    <item>
      <title>USB support at u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402906#M59679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am seeing that u-boot - 2013.04 has support for u-boot but what are the prerequisites that are needed to make the boot possible from USB device? Does anybody have an idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; usb start&lt;/P&gt;&lt;P&gt;(Re)start USB...&lt;/P&gt;&lt;P&gt;USB0:&amp;nbsp;&amp;nbsp; USB EHCI 1.00&lt;/P&gt;&lt;P&gt;scanning bus 0 for devices... 1 USB Device(s) found&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scanning usb for storage devices... 0 Storage Device(s) found&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scanning usb for ethernet devices... 0 Ethernet Device(s) found&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are the logs found on my board even though i have connected USB stick on HOST1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Sep 2015 12:11:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402906#M59679</guid>
      <dc:creator>manjunathjoshi</dc:creator>
      <dc:date>2015-09-24T12:11:20Z</dc:date>
    </item>
    <item>
      <title>Re: USB support at u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402907#M59680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manju&lt;/P&gt;&lt;P&gt;What board is this ? Also, can you just try a more&lt;/P&gt;&lt;P&gt;recent (and preferably a mainline) u-boot version.&lt;/P&gt;&lt;P&gt;On my sabresd board, with mainline u-boot from&lt;/P&gt;&lt;P&gt;tip of the mainline tree, USB works fine.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Sep 2015 17:22:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402907#M59680</guid>
      <dc:creator>sinanakman</dc:creator>
      <dc:date>2015-09-24T17:22:31Z</dc:date>
    </item>
    <item>
      <title>Re: USB support at u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402908#M59681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manju,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just to clarify: mx6 does not boot from directly USB thumb. Is this what you are trying to achieve?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to flash U-boot in to one of the supported media: SD/eMMC, SPI NOR, SATA, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The usb support command in U-boot allows you to connect USB thumb and you can read files from it, but you cannot boot U-boot from a USB thumb.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Sep 2015 22:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402908#M59681</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2015-09-24T22:20:19Z</dc:date>
    </item>
    <item>
      <title>Re: USB support at u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402909#M59682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sinan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply. The board is custom one similar to SABRESD but has 2 USB hosts. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are right. With mainline u-boot which i have, the USB is supported. I can see in the u-boot prompt. Apart from that what should i take care off in the source so that the USB device is detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is, when i connect USB i see that power is not going to the device. We can see the USB LED blinking as soon as the kernel boots up but not at the u-boot prompt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2015 06:12:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402909#M59682</guid>
      <dc:creator>manjunathjoshi</dc:creator>
      <dc:date>2015-09-25T06:12:42Z</dc:date>
    </item>
    <item>
      <title>Re: USB support at u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402910#M59683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fabio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My intention is to boot the kernel and filesystem from u-boot prompt through USB. The board already has u-boot in eMMC. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2015 06:16:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402910#M59683</guid>
      <dc:creator>manjunathjoshi</dc:creator>
      <dc:date>2015-09-25T06:16:26Z</dc:date>
    </item>
    <item>
      <title>Re: USB support at u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402911#M59684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manju,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uboot usb is supported since 3.10.17 bsp release.&lt;/P&gt;&lt;P&gt;But here is the concern. The usb stack in uboot is very old and weak.&lt;/P&gt;&lt;P&gt;lots of usb stick cannot be used. Most of them can not be used is new usb stick.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2015 07:38:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402911#M59684</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2015-09-25T07:38:54Z</dc:date>
    </item>
    <item>
      <title>Re: USB support at u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402912#M59685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB is connected to a hub and then to the processor. That is why i was not able to see the LED blinking or the storage device. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now i am able to see in other similar board with no hub. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So if anyone using the USB, has to make sure that the lines are connected to i-mx directly since i-mx has dedicated USB port connection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2015 11:12:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-support-at-u-boot/m-p/402912#M59685</guid>
      <dc:creator>manjunathjoshi</dc:creator>
      <dc:date>2015-09-25T11:12:49Z</dc:date>
    </item>
  </channel>
</rss>