<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 bitbake yocto question</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-yocto-question/m-p/402849#M59665</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;WARNING: Failed to fetch URL &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true" rel="nofollow"&gt;http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true&lt;/A&gt;&lt;SPAN&gt;, attempting MIRRORS if available&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;ERROR: Fetcher failure: Fetch command failed with exit code 8, output:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin:" rel="nofollow"&gt;http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin:&lt;/A&gt;&lt;/P&gt;&lt;P&gt;2015-07-13 09:22:58 ERROR 404: Not Found.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;ERROR: Function failed: Fetcher failure for URL: '&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true" rel="nofollow"&gt;http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true&lt;/A&gt;&lt;SPAN&gt;'. Unable to fetch URL from any source.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/jishuxing/fsl-arm-yocto-bsp/build/tmp/work/riotboard-poky-linux-gnueabi/imx-test-hdcp/3.10.17-1.0.0-r0/temp/log.do_fetch.3692&lt;/P&gt;&lt;P&gt;ERROR: Task 1667 (/home/jishuxing/fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/imx-test/imx-test-hdcp_3.10.17-1.0.0.bb, do_fetch) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 2351 tasks of which 2350 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;No currently running tasks (2350 of 4013)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jul 2015 02:09:43 GMT</pubDate>
    <dc:creator>hnxylhb</dc:creator>
    <dc:date>2015-07-13T02:09:43Z</dc:date>
    <item>
      <title>bitbake yocto question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-yocto-question/m-p/402849#M59665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;WARNING: Failed to fetch URL &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true" rel="nofollow"&gt;http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true&lt;/A&gt;&lt;SPAN&gt;, attempting MIRRORS if available&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;ERROR: Fetcher failure: Fetch command failed with exit code 8, output:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin:" rel="nofollow"&gt;http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin:&lt;/A&gt;&lt;/P&gt;&lt;P&gt;2015-07-13 09:22:58 ERROR 404: Not Found.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;ERROR: Function failed: Fetcher failure for URL: '&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true" rel="nofollow"&gt;http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true&lt;/A&gt;&lt;SPAN&gt;'. Unable to fetch URL from any source.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/jishuxing/fsl-arm-yocto-bsp/build/tmp/work/riotboard-poky-linux-gnueabi/imx-test-hdcp/3.10.17-1.0.0-r0/temp/log.do_fetch.3692&lt;/P&gt;&lt;P&gt;ERROR: Task 1667 (/home/jishuxing/fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/imx-test/imx-test-hdcp_3.10.17-1.0.0.bb, do_fetch) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 2351 tasks of which 2350 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;No currently running tasks (2350 of 4013)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2015 02:09:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-yocto-question/m-p/402849#M59665</guid>
      <dc:creator>hnxylhb</dc:creator>
      <dc:date>2015-07-13T02:09:43Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake yocto question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-yocto-question/m-p/402850#M59666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello roc li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please provide more information on this error? Which BSP are you using and which images or packages are you baking? I’m curious because the binaries are not being downloaded from the gits but from Freescale.com&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2015 21:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-yocto-question/m-p/402850#M59666</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-07-14T21:59:25Z</dc:date>
    </item>
  </channel>
</rss>