<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQuestion, i.MX6D/Q CSI input capability</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6D-Q-CSI-input-capability/m-p/402829#M59657</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about the CSI camera input capability of i.MX6DQ.&lt;/P&gt;&lt;P&gt;When my customer tried to capture Full-HD video from OV5640 camera module connected to i.MX6Q-SABRE board,&lt;/P&gt;&lt;P&gt;they saw the message which indicate that the maximum frame rate is limited to 15fps.&lt;/P&gt;&lt;P&gt;They believe that the maximum frame rate limitation comes from the specification of OV5640 module.&lt;/P&gt;&lt;P&gt;And they believe that the capability of i.MX6DQ/CSI, paralle CSI input, is higher than that.&lt;/P&gt;&lt;P&gt;Are they correct?&lt;/P&gt;&lt;P&gt;Let me ask one more.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;They think the video capturing at Full-HD/30fps using with CSI parallel input is rarely done in general. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;They think most of the implementation for the video capturing at Full-HD/30fps is done by using with MIPI, not parallel input, in general.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Are they right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Oct 2015 11:20:28 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2015-10-16T11:20:28Z</dc:date>
    <item>
      <title>Question, i.MX6D/Q CSI input capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6D-Q-CSI-input-capability/m-p/402829#M59657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about the CSI camera input capability of i.MX6DQ.&lt;/P&gt;&lt;P&gt;When my customer tried to capture Full-HD video from OV5640 camera module connected to i.MX6Q-SABRE board,&lt;/P&gt;&lt;P&gt;they saw the message which indicate that the maximum frame rate is limited to 15fps.&lt;/P&gt;&lt;P&gt;They believe that the maximum frame rate limitation comes from the specification of OV5640 module.&lt;/P&gt;&lt;P&gt;And they believe that the capability of i.MX6DQ/CSI, paralle CSI input, is higher than that.&lt;/P&gt;&lt;P&gt;Are they correct?&lt;/P&gt;&lt;P&gt;Let me ask one more.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;They think the video capturing at Full-HD/30fps using with CSI parallel input is rarely done in general. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;They think most of the implementation for the video capturing at Full-HD/30fps is done by using with MIPI, not parallel input, in general.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Are they right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 11:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6D-Q-CSI-input-capability/m-p/402829#M59657</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-10-16T11:20:28Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6D/Q CSI input capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6D-Q-CSI-input-capability/m-p/402830#M59658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Miyamoto&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are correct, capability of i.MX6DQ/CSI parallel CSI input is higher,&lt;/P&gt;&lt;P&gt;15fps limit comes from OV5640 as coefficient tables are given by its vendor and &lt;/P&gt;&lt;P&gt;under NDA with them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;They think most of the implementation for the video capturing at Full-HD/30fps&lt;/P&gt;&lt;P&gt;&amp;gt;is done by using with MIPI, not parallel input, in general.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Oct 2015 02:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6D-Q-CSI-input-capability/m-p/402830#M59658</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-10-17T02:03:14Z</dc:date>
    </item>
  </channel>
</rss>