<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: WatchDog_B pin is not getting asserted</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/WatchDog-B-pin-is-not-getting-asserted/m-p/402628#M59626</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Issue is resolved &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reason for Issue:&lt;/P&gt;&lt;P&gt; Configured the MUx control of&amp;nbsp; DISP0_DATA08&amp;nbsp; to WDOG1_B, but doesn't configured pad control registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WCR= 0x779F;&lt;/P&gt;&lt;P&gt; In above initialization&amp;nbsp; WDA bit is cleared.&lt;/P&gt;&lt;P&gt; So WDOG1_B pin get asserted, once I Configured DISP0_DATA08 PAD and MUX control registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fix: &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Configure DISP0_DATA08 PAD and MUX control registers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Set WDA bit to 1,&amp;nbsp; so it behaves in system default mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; WCR = 0x77BF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; After above fix WDOG1_B pin gets asserted whenever&amp;nbsp; watch dog timeout happens or SRS bit is cleared.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Aug 2015 14:28:11 GMT</pubDate>
    <dc:creator>arunvarma</dc:creator>
    <dc:date>2015-08-28T14:28:11Z</dc:date>
    <item>
      <title>WatchDog_B pin is not getting asserted</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WatchDog-B-pin-is-not-getting-asserted/m-p/402627#M59625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt; I am using custom board based on SaberSD design (processor imx6dl). &lt;/P&gt;&lt;P&gt; Using Watchdog_1&amp;nbsp; for timeout and reset, IPU1_DISP0_DATA08 / IPU2_DISP0_DATA08 / PWM1_OUT / WDOG1_B / &amp;lt;GPIO4_IO29&amp;gt; in is connected to PMIC reset pin.&lt;/P&gt;&lt;P&gt;If SRS bit is cleared / watchdog time out happens OS get restarted, but WATCHDOG1_B is not asserted( so no power reset happens).&lt;/P&gt;&lt;P&gt;WCR is initialized&amp;nbsp; to 0x779f.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Aug 2015 09:16:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WatchDog-B-pin-is-not-getting-asserted/m-p/402627#M59625</guid>
      <dc:creator>arunvarma</dc:creator>
      <dc:date>2015-08-27T09:16:35Z</dc:date>
    </item>
    <item>
      <title>Re: WatchDog_B pin is not getting asserted</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WatchDog-B-pin-is-not-getting-asserted/m-p/402628#M59626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Issue is resolved &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reason for Issue:&lt;/P&gt;&lt;P&gt; Configured the MUx control of&amp;nbsp; DISP0_DATA08&amp;nbsp; to WDOG1_B, but doesn't configured pad control registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WCR= 0x779F;&lt;/P&gt;&lt;P&gt; In above initialization&amp;nbsp; WDA bit is cleared.&lt;/P&gt;&lt;P&gt; So WDOG1_B pin get asserted, once I Configured DISP0_DATA08 PAD and MUX control registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fix: &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Configure DISP0_DATA08 PAD and MUX control registers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Set WDA bit to 1,&amp;nbsp; so it behaves in system default mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; WCR = 0x77BF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; After above fix WDOG1_B pin gets asserted whenever&amp;nbsp; watch dog timeout happens or SRS bit is cleared.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2015 14:28:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WatchDog-B-pin-is-not-getting-asserted/m-p/402628#M59626</guid>
      <dc:creator>arunvarma</dc:creator>
      <dc:date>2015-08-28T14:28:11Z</dc:date>
    </item>
  </channel>
</rss>