<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Ethernet failure issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-failure-issue/m-p/402616#M59616</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am testing a board based on i.MX6Q processor. in that ethernet ping test is failed. The component mounting is done as per the&amp;nbsp; schematics. And every voltage , clock frequency are proper. Please suggest the solution.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 11 Jul 2015 06:14:47 GMT</pubDate>
    <dc:creator>vineethhegde</dc:creator>
    <dc:date>2015-07-11T06:14:47Z</dc:date>
    <item>
      <title>Ethernet failure issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-failure-issue/m-p/402616#M59616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am testing a board based on i.MX6Q processor. in that ethernet ping test is failed. The component mounting is done as per the&amp;nbsp; schematics. And every voltage , clock frequency are proper. Please suggest the solution.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jul 2015 06:14:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-failure-issue/m-p/402616#M59616</guid>
      <dc:creator>vineethhegde</dc:creator>
      <dc:date>2015-07-11T06:14:47Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet failure issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-failure-issue/m-p/402617#M59617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi vineeth113&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;first check 125MHz clock, it should be outputed from ethernet phy and should have &lt;/P&gt;&lt;P&gt;correct duty cycle, if not, then you have to use a 125MHz oscillator for both i.MX6 &lt;/P&gt;&lt;P&gt;and phy, the tolerance is +/-50ppm. Please check timings described in sect.4.11.5.3&lt;/P&gt;&lt;P&gt;RGMII Signal Switching Specifications &lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQCEC &lt;/A&gt;with oscilloscope&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/526454"&gt;ENET_REF_CLK (ball V22) duty-cycle requirements on i.MX6&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2015 12:01:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-failure-issue/m-p/402617#M59617</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-13T12:01:16Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet failure issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-failure-issue/m-p/402618#M59618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;in that same board Ethernet phy IC is replaced then also issue persist.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 07:07:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-failure-issue/m-p/402618#M59618</guid>
      <dc:creator>vineethhegde</dc:creator>
      <dc:date>2015-07-15T07:07:00Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet failure issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-failure-issue/m-p/402619#M59619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;measure Ethernet phy timings using oscilloscope and&lt;/P&gt;&lt;P&gt;check with datasheet requirements&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 12:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-failure-issue/m-p/402619#M59619</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-15T12:50:33Z</dc:date>
    </item>
  </channel>
</rss>