<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX28 : EMI pin keeper function</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-EMI-pin-keeper-function/m-p/402326#M59539</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We design the custom board .&lt;BR /&gt;We need information about EMI pin behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The EMI pin is&amp;nbsp; EMI_ODT1, EMI_CE1N. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The register setting is as follows.&lt;BR /&gt;&amp;nbsp; HW_PINCTRL_MUXSELxx = 11 ( function disable ) &lt;BR /&gt;&amp;nbsp; PINCTRL Bank 5/6 Pad Keeper Disable Register = 0 ( enable the internal keeper)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question1.&lt;BR /&gt;&amp;nbsp; Is the internal keeper function enabled ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question2.&lt;BR /&gt;&amp;nbsp; If the "PINCTRL Bank 5/6 Pad Keeper Disable Register"&amp;nbsp; set as "1" ( disable the internal keeper),&lt;BR /&gt;&amp;nbsp; then, Is the pin state high impedance ?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards, &lt;BR /&gt;Koichi Sakagami &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jun 2015 06:30:23 GMT</pubDate>
    <dc:creator>koichisakagami</dc:creator>
    <dc:date>2015-06-16T06:30:23Z</dc:date>
    <item>
      <title>iMX28 : EMI pin keeper function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-EMI-pin-keeper-function/m-p/402326#M59539</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We design the custom board .&lt;BR /&gt;We need information about EMI pin behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The EMI pin is&amp;nbsp; EMI_ODT1, EMI_CE1N. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The register setting is as follows.&lt;BR /&gt;&amp;nbsp; HW_PINCTRL_MUXSELxx = 11 ( function disable ) &lt;BR /&gt;&amp;nbsp; PINCTRL Bank 5/6 Pad Keeper Disable Register = 0 ( enable the internal keeper)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question1.&lt;BR /&gt;&amp;nbsp; Is the internal keeper function enabled ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question2.&lt;BR /&gt;&amp;nbsp; If the "PINCTRL Bank 5/6 Pad Keeper Disable Register"&amp;nbsp; set as "1" ( disable the internal keeper),&lt;BR /&gt;&amp;nbsp; then, Is the pin state high impedance ?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards, &lt;BR /&gt;Koichi Sakagami &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2015 06:30:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-EMI-pin-keeper-function/m-p/402326#M59539</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2015-06-16T06:30:23Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 : EMI pin keeper function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-EMI-pin-keeper-function/m-p/402327#M59540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; The internal keeper function is enabled.&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;According to Figure 9-1 (Pad Diagram) of the i.MX28 Reference Manual &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;the internal keeper can be enabled / disabled separately, without reference &lt;BR /&gt;to multiplexing options. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;2.&lt;BR /&gt; From section 9.1 (Pin Control and GPIO Overview) :&lt;BR /&gt; “All EMI pins' internal keepers can be disabled to allow them to change to &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;a high impedance state […]”.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2015 07:04:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-EMI-pin-keeper-function/m-p/402327#M59540</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-06-16T07:04:19Z</dc:date>
    </item>
  </channel>
</rss>