<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using only one ddr3 sdram chip(two byte group) for i.MX6 processors in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-only-one-ddr3-sdram-chip-two-byte-group-for-i-MX6/m-p/401479#M59311</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tingam&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes one can use 16 bit configuration MMDC_MDCTL, DSIZ=0 16-bit data bus,&lt;/P&gt;&lt;P&gt;as two byte group or one ddr3 IC connected to imx6sl processer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Oct 2015 06:33:48 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-10-16T06:33:48Z</dc:date>
    <item>
      <title>Using only one ddr3 sdram chip(two byte group) for i.MX6 processors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-only-one-ddr3-sdram-chip-two-byte-group-for-i-MX6/m-p/401478#M59310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm wondering if it is ok to just use two byte group or one ddr3 IC connected to imx6sl processer? I want to only have 2GB ram for my board and I want to use a single chip for it, instead of 2x1GB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 02:52:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-only-one-ddr3-sdram-chip-two-byte-group-for-i-MX6/m-p/401478#M59310</guid>
      <dc:creator>tinganho</dc:creator>
      <dc:date>2015-10-16T02:52:18Z</dc:date>
    </item>
    <item>
      <title>Re: Using only one ddr3 sdram chip(two byte group) for i.MX6 processors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-only-one-ddr3-sdram-chip-two-byte-group-for-i-MX6/m-p/401479#M59311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tingam&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes one can use 16 bit configuration MMDC_MDCTL, DSIZ=0 16-bit data bus,&lt;/P&gt;&lt;P&gt;as two byte group or one ddr3 IC connected to imx6sl processer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 06:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-only-one-ddr3-sdram-chip-two-byte-group-for-i-MX6/m-p/401479#M59311</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-10-16T06:33:48Z</dc:date>
    </item>
  </channel>
</rss>