<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: LCD INTERFACE WITH IMX6 SABRE</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LCD-INTERFACE-WITH-IMX6-SABRE/m-p/401408#M59306</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The solution you consider seems to be the working one. You then have to adjust the screen resolution parameters in display driver and correctly handle the touchscreen by I2C interface.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Sep 2015 09:41:03 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2015-09-10T09:41:03Z</dc:date>
    <item>
      <title>LCD INTERFACE WITH IMX6 SABRE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-INTERFACE-WITH-IMX6-SABRE/m-p/401407#M59305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are planning to use "&lt;STRONG&gt;BD070LIC1 – 7″ 1280×800 Display&lt;/STRONG&gt;" with Touchscreen for our project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The connectors in the LCD + Touchscreen is not compatible with our host board, So we have decided to use a intermediate connector board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Details of the host board :&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Freescale i.MX6 Sabre SDP&lt;/LI&gt;&lt;LI&gt;Android 5.0.1&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find attached schematics, Can anyone please make sure the LCD will work with Sabre SDP. Also recommend if any other 7" LVDS LCD is compatible for our host board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ref:&lt;/P&gt;&lt;P&gt;Host board - &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT"&gt;SABRE for Smart Devices Reference Design|Freescale&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Original present Working LCD - &lt;A href="http://boundarydevices.com/wp-content/uploads/2013/06/HSD100PXN1-A00-C11-1.0.pdf" target="_blank"&gt;http://boundarydevices.com/wp-content/uploads/2013/06/HSD100PXN1-A00-C11-1.0.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LCD we are going to use - &lt;A href="http://boundarydevices.com/wp-content/uploads/2014/12/HSD070PWW1-B01.pdf" target="_blank"&gt;http://boundarydevices.com/wp-content/uploads/2014/12/HSD070PWW1-B01.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Touchscreen we are going to use - &lt;A&gt;http://boundarydevices.com/wp-content/uploads/2015/05/SE-CTPGG7007.pdf#page=1&amp;amp;zoom=170,402,836&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Venkat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Aug 2015 06:37:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-INTERFACE-WITH-IMX6-SABRE/m-p/401407#M59305</guid>
      <dc:creator>venkat_c</dc:creator>
      <dc:date>2015-08-27T06:37:25Z</dc:date>
    </item>
    <item>
      <title>Re: LCD INTERFACE WITH IMX6 SABRE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-INTERFACE-WITH-IMX6-SABRE/m-p/401408#M59306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The solution you consider seems to be the working one. You then have to adjust the screen resolution parameters in display driver and correctly handle the touchscreen by I2C interface.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Sep 2015 09:41:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-INTERFACE-WITH-IMX6-SABRE/m-p/401408#M59306</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-09-10T09:41:03Z</dc:date>
    </item>
  </channel>
</rss>