<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックWriting mmcblk0boot0 partition from linux command line</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Writing-mmcblk0boot0-partition-from-linux-command-line/m-p/400070#M58990</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to update the u-boot on my iMX6 board without having to open the packaging.&amp;nbsp; I have access to unit via network and the android adb tool so I can get console access and can stage the u-boot binary in the mounted MMC partition.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see that the u-boot is programmed into the /dev/block/mmcblk0boot0 and /dev/block/mmcblk0boot1 block devices.&amp;nbsp;&amp;nbsp; However, when I try to dd the new image to those partitions I get the following response: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# dd if=/sdcard/uboot.bin of=/dev/block/mmcblk0boot0 seek=1024&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/dev/block/mmcblk0boot0: write error: Operation not permitted&lt;/P&gt;&lt;P&gt;1+0 records in&lt;/P&gt;&lt;P&gt;0+0 records out&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried opening up the permissions on the /dev/block/mmcblk0boot0 device with no luck.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this even possible?&amp;nbsp; Do I need to change something in how the kernel image is built or how it is initially programmed?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;P&gt;Doug Bailey &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Nov 2015 22:52:07 GMT</pubDate>
    <dc:creator>dougbailey</dc:creator>
    <dc:date>2015-11-10T22:52:07Z</dc:date>
    <item>
      <title>Writing mmcblk0boot0 partition from linux command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Writing-mmcblk0boot0-partition-from-linux-command-line/m-p/400070#M58990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to update the u-boot on my iMX6 board without having to open the packaging.&amp;nbsp; I have access to unit via network and the android adb tool so I can get console access and can stage the u-boot binary in the mounted MMC partition.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see that the u-boot is programmed into the /dev/block/mmcblk0boot0 and /dev/block/mmcblk0boot1 block devices.&amp;nbsp;&amp;nbsp; However, when I try to dd the new image to those partitions I get the following response: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# dd if=/sdcard/uboot.bin of=/dev/block/mmcblk0boot0 seek=1024&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/dev/block/mmcblk0boot0: write error: Operation not permitted&lt;/P&gt;&lt;P&gt;1+0 records in&lt;/P&gt;&lt;P&gt;0+0 records out&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried opening up the permissions on the /dev/block/mmcblk0boot0 device with no luck.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this even possible?&amp;nbsp; Do I need to change something in how the kernel image is built or how it is initially programmed?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;P&gt;Doug Bailey &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Nov 2015 22:52:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Writing-mmcblk0boot0-partition-from-linux-command-line/m-p/400070#M58990</guid>
      <dc:creator>dougbailey</dc:creator>
      <dc:date>2015-11-10T22:52:07Z</dc:date>
    </item>
    <item>
      <title>Re: Writing mmcblk0boot0 partition from linux command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Writing-mmcblk0boot0-partition-from-linux-command-line/m-p/400071#M58991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It appears that the answer would be in the linux documentation.&lt;/P&gt;&lt;P&gt; &lt;A href="https://www.kernel.org/doc/Documentation/mmc/mmc-dev-parts.txt" title="https://www.kernel.org/doc/Documentation/mmc/mmc-dev-parts.txt"&gt;https://www.kernel.org/doc/Documentation/mmc/mmc-dev-parts.txt&amp;nbsp; &lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Nov 2015 22:31:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Writing-mmcblk0boot0-partition-from-linux-command-line/m-p/400071#M58991</guid>
      <dc:creator>dougbailey</dc:creator>
      <dc:date>2015-11-11T22:31:12Z</dc:date>
    </item>
  </channel>
</rss>