<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Pixel distortion with X11 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Pixel-distortion-with-X11/m-p/399894#M58938</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have board with i.MX6 cpu and 7" lcd display, connected as parallel rgb (18-bit).&lt;/P&gt;&lt;P&gt;When i run the vivante samples as native open gl with framebuffer, it's all ok. The samples where shown on the display as expected.&lt;/P&gt;&lt;P&gt;But when I try to work with the X11 server i get heavy pixel distortion. It looks like the bpp used by X11 does not match the bpp of the lcd.&lt;/P&gt;&lt;P&gt;I tried already to change the 'DefaultDepth' value in the xorg.conf, but with no success.&lt;/P&gt;&lt;P&gt;The same problems appear in Yocto (Dora) with X-server version 1.14 and Ubuntu 12.04 with X-sever vesrion 1.11.&lt;/P&gt;&lt;P&gt;Also the distortion is not static, the pixels are flickering.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below you see an picture of what i mean. The background should be a simple linear gradient from red to green.&lt;/P&gt;&lt;P&gt;I think it's a problem with the X-server because if i stop the server (for Example with 'service lightdm stop' in Ubuntu) the distortion stops and the background is shown as a smooth gradient.&lt;/P&gt;&lt;P&gt;It affects not only the background, also the icons, scrollbars, borders, etc.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="IMAG0168.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49620iBDDAE834F2119893/image-size/large?v=v2&amp;amp;px=999" role="button" title="IMAG0168.jpg" alt="IMAG0168.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone has an idea to solve this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 12 Apr 2015 07:57:55 GMT</pubDate>
    <dc:creator>philippt85</dc:creator>
    <dc:date>2015-04-12T07:57:55Z</dc:date>
    <item>
      <title>Pixel distortion with X11</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pixel-distortion-with-X11/m-p/399894#M58938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have board with i.MX6 cpu and 7" lcd display, connected as parallel rgb (18-bit).&lt;/P&gt;&lt;P&gt;When i run the vivante samples as native open gl with framebuffer, it's all ok. The samples where shown on the display as expected.&lt;/P&gt;&lt;P&gt;But when I try to work with the X11 server i get heavy pixel distortion. It looks like the bpp used by X11 does not match the bpp of the lcd.&lt;/P&gt;&lt;P&gt;I tried already to change the 'DefaultDepth' value in the xorg.conf, but with no success.&lt;/P&gt;&lt;P&gt;The same problems appear in Yocto (Dora) with X-server version 1.14 and Ubuntu 12.04 with X-sever vesrion 1.11.&lt;/P&gt;&lt;P&gt;Also the distortion is not static, the pixels are flickering.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below you see an picture of what i mean. The background should be a simple linear gradient from red to green.&lt;/P&gt;&lt;P&gt;I think it's a problem with the X-server because if i stop the server (for Example with 'service lightdm stop' in Ubuntu) the distortion stops and the background is shown as a smooth gradient.&lt;/P&gt;&lt;P&gt;It affects not only the background, also the icons, scrollbars, borders, etc.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="IMAG0168.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49620iBDDAE834F2119893/image-size/large?v=v2&amp;amp;px=999" role="button" title="IMAG0168.jpg" alt="IMAG0168.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone has an idea to solve this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Apr 2015 07:57:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pixel-distortion-with-X11/m-p/399894#M58938</guid>
      <dc:creator>philippt85</dc:creator>
      <dc:date>2015-04-12T07:57:55Z</dc:date>
    </item>
    <item>
      <title>Re: Pixel distortion with X11</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pixel-distortion-with-X11/m-p/399895#M58939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Philipp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would sggest try new BSP&amp;nbsp; with GPU driver upgraded to Vivante v5.0.11p4.4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.14.28_1.0.0_iMX6QDLS_BUNDLE&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,&lt;/P&gt;&lt;P&gt;i.MX 6Solo Linux Binary Demo Files and Linux BSP&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Apr 2015 07:41:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pixel-distortion-with-X11/m-p/399895#M58939</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-13T07:41:13Z</dc:date>
    </item>
    <item>
      <title>Re: Pixel distortion with X11</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pixel-distortion-with-X11/m-p/399896#M58940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;i can't switch to a newer BSP. I have to use a given kernel which is a 3.0.35 with support for vivante 4.6.9p12.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried software rendering for X11, with the same result...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Apr 2015 08:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pixel-distortion-with-X11/m-p/399896#M58940</guid>
      <dc:creator>philippt85</dc:creator>
      <dc:date>2015-04-13T08:26:35Z</dc:date>
    </item>
  </channel>
</rss>