<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MPF0100F0ANES pmic not replying on i2c</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MPF0100F0ANES-pmic-not-replying-on-i2c/m-p/399707#M58877</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor, &lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;i have several devices in the bus, working properly. Only PMIC is not responding, so i would exclude any imx6q pinmux issue.&lt;/P&gt;&lt;P&gt;VIN is 3V3, VDDIO is 3v3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible some of this chip are programmed on OTP without i2c enabled ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Angelo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Oct 2015 08:15:47 GMT</pubDate>
    <dc:creator>angelo_d</dc:creator>
    <dc:date>2015-10-16T08:15:47Z</dc:date>
    <item>
      <title>MPF0100F0ANES pmic not replying on i2c</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MPF0100F0ANES-pmic-not-replying-on-i2c/m-p/399705#M58875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;did a small linux tool for i2c, and (unless i have no bugs, that shouldn't be since all other devices in the bus are detected correctly) looks like the PMIC is not replying. It should reply at a 0x08 address, or near it.&lt;/P&gt;&lt;P&gt;We should need to control some voltage so if possible i would understand what is wrong here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reagrds&lt;/P&gt;&lt;P&gt;Angelo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Oct 2015 08:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MPF0100F0ANES-pmic-not-replying-on-i2c/m-p/399705#M58875</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2015-10-15T08:28:42Z</dc:date>
    </item>
    <item>
      <title>Re: MPF0100F0ANES pmic not replying on i2c</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MPF0100F0ANES-pmic-not-replying-on-i2c/m-p/399706#M58876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi angelo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check i2c iomux settings and if SION bit is set in&lt;/P&gt;&lt;P&gt;IOMUXC_SW_MUX_CTL register. As for PMIC, to communicate with I2C,&lt;/P&gt;&lt;P&gt;VIN must be valid and VDDIO, to which SDA and SCL are pulled up, must be&lt;/P&gt;&lt;P&gt;powered by a 1.7 to 3.6 V supply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 01:56:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MPF0100F0ANES-pmic-not-replying-on-i2c/m-p/399706#M58876</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-10-16T01:56:14Z</dc:date>
    </item>
    <item>
      <title>Re: MPF0100F0ANES pmic not replying on i2c</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MPF0100F0ANES-pmic-not-replying-on-i2c/m-p/399707#M58877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor, &lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;i have several devices in the bus, working properly. Only PMIC is not responding, so i would exclude any imx6q pinmux issue.&lt;/P&gt;&lt;P&gt;VIN is 3V3, VDDIO is 3v3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible some of this chip are programmed on OTP without i2c enabled ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Angelo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 08:15:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MPF0100F0ANES-pmic-not-replying-on-i2c/m-p/399707#M58877</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2015-10-16T08:15:47Z</dc:date>
    </item>
    <item>
      <title>Re: MPF0100F0ANES pmic not replying on i2c</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MPF0100F0ANES-pmic-not-replying-on-i2c/m-p/399708#M58878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi angelo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i2c can not be disabled. Is this one chip or several,&lt;/P&gt;&lt;P&gt;had you checked signals with oscilloscope?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 09:15:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MPF0100F0ANES-pmic-not-replying-on-i2c/m-p/399708#M58878</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-10-16T09:15:46Z</dc:date>
    </item>
  </channel>
</rss>