<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6SX ref design / kernel support for 14x14 package ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SX-ref-design-kernel-support-for-14x14-package/m-p/399302#M58767</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stuart.&lt;/P&gt;&lt;P&gt;Attached you could find the symbols and footprints for the i.MX6SX in MAPBGA400 package (14x14).&lt;/P&gt;&lt;P&gt;Regarding the DTB, you could use as reference the DTS from the official BSPs, and removing the modules that are not included on the target package, for compiling and generating a proper DTB file.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Oct 2015 18:41:25 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2015-10-20T18:41:25Z</dc:date>
    <item>
      <title>IMX6SX ref design / kernel support for 14x14 package ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SX-ref-design-kernel-support-for-14x14-package/m-p/399301#M58766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a reference design / schematics symbols for the IMX6SX (Solo X) in the 14x14 package ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also what about a kernel DTS/DTB file for the 14x14 package ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looks like u-boot supports it (make mx6sx_14x14_lpddr2_arm2_defconfig) ....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I do not see any imx6sx-14x14... dts files in the kernel tree under arch/arm/boot/dts&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 19:29:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6SX-ref-design-kernel-support-for-14x14-package/m-p/399301#M58766</guid>
      <dc:creator>SJA</dc:creator>
      <dc:date>2015-10-14T19:29:27Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6SX ref design / kernel support for 14x14 package ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SX-ref-design-kernel-support-for-14x14-package/m-p/399302#M58767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stuart.&lt;/P&gt;&lt;P&gt;Attached you could find the symbols and footprints for the i.MX6SX in MAPBGA400 package (14x14).&lt;/P&gt;&lt;P&gt;Regarding the DTB, you could use as reference the DTS from the official BSPs, and removing the modules that are not included on the target package, for compiling and generating a proper DTB file.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Oct 2015 18:41:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6SX-ref-design-kernel-support-for-14x14-package/m-p/399302#M58767</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-10-20T18:41:25Z</dc:date>
    </item>
  </channel>
</rss>