<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピック[solved]imx6 USB Camera</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/solved-imx6-USB-Camera/m-p/398349#M58523</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm trying build an image yocto with gstreamer. I added on local.conf file the IMAGE_INSTALL_append:&amp;nbsp; "gst-plugins-base-meta gst-plugins-good-meta gst-ffmpeg gst-fsl-plugin" modules, and executed the process from this link: &lt;/SPAN&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="93688" data-objecttype="102" href="https://community.nxp.com/docs/DOC-93688"&gt;https://community.freescale.com/docs/DOC-93688&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The output from the command&amp;nbsp; "gst-launch v4l2src ! mfw_v4lsink" is:&lt;/P&gt;&lt;P&gt;root@cgtqmx6:~# gst-launch v4l2src ! mfw_v4lsink&lt;/P&gt;&lt;P&gt;MFW_GST_V4LSINK_PLUGIN 3.0.11 build on Jul 30 2015 17:48:50.&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;/P&gt;&lt;P&gt;ERROR: Pipeline doesn't want to pause.&lt;/P&gt;&lt;P&gt;ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Cannot identify device '/dev/video0'.&lt;/P&gt;&lt;P&gt;Additional debug info:&lt;/P&gt;&lt;P&gt;/home/polosulorg/yocto/bsp-scripts/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gst-plugins-good/0.10.31-r8/gst-plugins-good-0.10.31/sys/v4l2/v4l2_calls.c(498): gst_v4l2_open (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:&lt;/P&gt;&lt;P&gt;system error: No such file or directory&lt;/P&gt;&lt;P&gt;Setting pipeline to NULL ...&lt;/P&gt;&lt;P&gt;Total rendered:0&lt;/P&gt;&lt;P&gt;Freeing pipeline ...&lt;/P&gt;&lt;P&gt;[---&amp;gt;FINALIZE v4l_sink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The device is not creating the /dev/video0. To create a new /dev/video0 I'm executing the command "mknod /dev/video0 c 81 0". After it, the output from the command "gst-launch v4l2src ! mfw_v4lsink" is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@cgtqmx6:~# gst-launch v4l2src ! mfw_v4lsink&lt;/P&gt;&lt;P&gt;MFW_GST_V4LSINK_PLUGIN 3.0.11 build on Jul 30 2015 17:48:50.&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;/P&gt;&lt;P&gt;ERROR: Pipeline doesn't want to pause.&lt;/P&gt;&lt;P&gt;ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Could not open device '/dev/video0' for reading and writing.&lt;/P&gt;&lt;P&gt;Additional debug info:&lt;/P&gt;&lt;P&gt;/home/polosulorg/yocto/bsp-scripts/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gst-plugins-good/0.10.31-r8/gst-plugins-good-0.10.31/sys/v4l2/v4l2_calls.c(512): gst_v4l2_open (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:&lt;/P&gt;&lt;P&gt;system error: No such device or address&lt;/P&gt;&lt;P&gt;Setting pipeline to NULL ...&lt;/P&gt;&lt;P&gt;Total rendered:0&lt;/P&gt;&lt;P&gt;Freeing pipeline ...&lt;/P&gt;&lt;P&gt;[---&amp;gt;FINALIZE v4l_sink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help-me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Jul 2015 22:50:51 GMT</pubDate>
    <dc:creator>mauriciokarrei</dc:creator>
    <dc:date>2015-07-30T22:50:51Z</dc:date>
    <item>
      <title>[solved]imx6 USB Camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/solved-imx6-USB-Camera/m-p/398349#M58523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm trying build an image yocto with gstreamer. I added on local.conf file the IMAGE_INSTALL_append:&amp;nbsp; "gst-plugins-base-meta gst-plugins-good-meta gst-ffmpeg gst-fsl-plugin" modules, and executed the process from this link: &lt;/SPAN&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="93688" data-objecttype="102" href="https://community.nxp.com/docs/DOC-93688"&gt;https://community.freescale.com/docs/DOC-93688&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The output from the command&amp;nbsp; "gst-launch v4l2src ! mfw_v4lsink" is:&lt;/P&gt;&lt;P&gt;root@cgtqmx6:~# gst-launch v4l2src ! mfw_v4lsink&lt;/P&gt;&lt;P&gt;MFW_GST_V4LSINK_PLUGIN 3.0.11 build on Jul 30 2015 17:48:50.&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;/P&gt;&lt;P&gt;ERROR: Pipeline doesn't want to pause.&lt;/P&gt;&lt;P&gt;ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Cannot identify device '/dev/video0'.&lt;/P&gt;&lt;P&gt;Additional debug info:&lt;/P&gt;&lt;P&gt;/home/polosulorg/yocto/bsp-scripts/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gst-plugins-good/0.10.31-r8/gst-plugins-good-0.10.31/sys/v4l2/v4l2_calls.c(498): gst_v4l2_open (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:&lt;/P&gt;&lt;P&gt;system error: No such file or directory&lt;/P&gt;&lt;P&gt;Setting pipeline to NULL ...&lt;/P&gt;&lt;P&gt;Total rendered:0&lt;/P&gt;&lt;P&gt;Freeing pipeline ...&lt;/P&gt;&lt;P&gt;[---&amp;gt;FINALIZE v4l_sink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The device is not creating the /dev/video0. To create a new /dev/video0 I'm executing the command "mknod /dev/video0 c 81 0". After it, the output from the command "gst-launch v4l2src ! mfw_v4lsink" is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@cgtqmx6:~# gst-launch v4l2src ! mfw_v4lsink&lt;/P&gt;&lt;P&gt;MFW_GST_V4LSINK_PLUGIN 3.0.11 build on Jul 30 2015 17:48:50.&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;/P&gt;&lt;P&gt;ERROR: Pipeline doesn't want to pause.&lt;/P&gt;&lt;P&gt;ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Could not open device '/dev/video0' for reading and writing.&lt;/P&gt;&lt;P&gt;Additional debug info:&lt;/P&gt;&lt;P&gt;/home/polosulorg/yocto/bsp-scripts/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gst-plugins-good/0.10.31-r8/gst-plugins-good-0.10.31/sys/v4l2/v4l2_calls.c(512): gst_v4l2_open (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:&lt;/P&gt;&lt;P&gt;system error: No such device or address&lt;/P&gt;&lt;P&gt;Setting pipeline to NULL ...&lt;/P&gt;&lt;P&gt;Total rendered:0&lt;/P&gt;&lt;P&gt;Freeing pipeline ...&lt;/P&gt;&lt;P&gt;[---&amp;gt;FINALIZE v4l_sink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help-me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2015 22:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/solved-imx6-USB-Camera/m-p/398349#M58523</guid>
      <dc:creator>mauriciokarrei</dc:creator>
      <dc:date>2015-07-30T22:50:51Z</dc:date>
    </item>
    <item>
      <title>Re: [solved]imx6 USB Camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/solved-imx6-USB-Camera/m-p/398350#M58524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem solved. I bought a new USB Camera with another driver. It's work perfectly.&lt;/P&gt;&lt;P&gt;Thank you so much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jul 2015 16:46:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/solved-imx6-USB-Camera/m-p/398350#M58524</guid>
      <dc:creator>mauriciokarrei</dc:creator>
      <dc:date>2015-07-31T16:46:28Z</dc:date>
    </item>
    <item>
      <title>Re: [solved]imx6 USB Camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/solved-imx6-USB-Camera/m-p/398351#M58525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mauricio Karrei,&lt;/P&gt;&lt;P&gt;I am very glad you have solved your problem. So I closed this thread, if you have any other questions you can create new threads in our community.&lt;/P&gt;&lt;P&gt;Have a nice day.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Aug 2015 02:52:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/solved-imx6-USB-Camera/m-p/398351#M58525</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2015-08-03T02:52:28Z</dc:date>
    </item>
    <item>
      <title>Re: [solved]imx6 USB Camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/solved-imx6-USB-Camera/m-p/398352#M58526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Mauricio Karrei&lt;BR /&gt;&lt;/SPAN&gt;&lt;BR /&gt;I got the exact same problem as you. What is the difference between the old one with the new one?&lt;BR /&gt;Could you please share the solution?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 02:41:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/solved-imx6-USB-Camera/m-p/398352#M58526</guid>
      <dc:creator>arkceajin</dc:creator>
      <dc:date>2017-06-12T02:41:26Z</dc:date>
    </item>
  </channel>
</rss>