<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: where is ssi's sys clock from?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/where-is-ssi-s-sys-clock-from/m-p/398337#M58518</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your answer,it is helpful to me.&lt;BR /&gt;But I have some other problem,can you help me ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I configure ssi1 as network mode,bit&amp;nbsp; clock and frame sync generated internally,and route ssi1 to AUD3.&lt;/P&gt;&lt;P&gt;But the bit clock and frame clock don't generate on AUD3!!! Why?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I output source of SSI1_CLK_ROOT on CLKO2 pin and sure it has started. The bit TXDIR also set 1 to output the clock.And the audmux configure as:&lt;/P&gt;&lt;P&gt;port 3 ptcr = 0x84000800&lt;/P&gt;&lt;P&gt;port 3 pdcr = 0x0&lt;/P&gt;&lt;P&gt;port 1 ptcr = 0x800&lt;/P&gt;&lt;P&gt;port 1 pdcr = 0x4000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where did I go wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards to you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Sep 2015 09:58:55 GMT</pubDate>
    <dc:creator>剑明廖</dc:creator>
    <dc:date>2015-09-22T09:58:55Z</dc:date>
    <item>
      <title>where is ssi's sys clock from?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/where-is-ssi-s-sys-clock-from/m-p/398335#M58516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53650i289DCA91197C510A/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In this figure we can see that ssi's bit clock comes from ssi's sys clock,but where is ssi's sys clock from?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What is the relationship between ssi's sys clock and ssi_clk_root?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We can found the ssi_clk_root in the following figure.(ssi1_clk_root、ssi2_clk_root、ssi3_clk_root).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53763i2834E877C8091DBD/image-size/large?v=v2&amp;amp;px=999" role="button" title="2.png" alt="2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 02:36:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/where-is-ssi-s-sys-clock-from/m-p/398335#M58516</guid>
      <dc:creator>剑明廖</dc:creator>
      <dc:date>2015-09-22T02:36:49Z</dc:date>
    </item>
    <item>
      <title>Re: where is ssi's sys clock from?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/where-is-ssi-s-sys-clock-from/m-p/398336#M58517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, the SSI sys clock and ssix_clk_root are the different wordings for the same thing. This sys clock comes from the clock controller module, it is ssi1_clk_root for the SSI1 module, ssi2_clk_root for the SSI2 module and ssi3_clk_root for the SSI3 module.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 09:07:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/where-is-ssi-s-sys-clock-from/m-p/398336#M58517</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-09-22T09:07:23Z</dc:date>
    </item>
    <item>
      <title>Re: where is ssi's sys clock from?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/where-is-ssi-s-sys-clock-from/m-p/398337#M58518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your answer,it is helpful to me.&lt;BR /&gt;But I have some other problem,can you help me ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I configure ssi1 as network mode,bit&amp;nbsp; clock and frame sync generated internally,and route ssi1 to AUD3.&lt;/P&gt;&lt;P&gt;But the bit clock and frame clock don't generate on AUD3!!! Why?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I output source of SSI1_CLK_ROOT on CLKO2 pin and sure it has started. The bit TXDIR also set 1 to output the clock.And the audmux configure as:&lt;/P&gt;&lt;P&gt;port 3 ptcr = 0x84000800&lt;/P&gt;&lt;P&gt;port 3 pdcr = 0x0&lt;/P&gt;&lt;P&gt;port 1 ptcr = 0x800&lt;/P&gt;&lt;P&gt;port 1 pdcr = 0x4000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where did I go wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards to you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 09:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/where-is-ssi-s-sys-clock-from/m-p/398337#M58518</guid>
      <dc:creator>剑明廖</dc:creator>
      <dc:date>2015-09-22T09:58:55Z</dc:date>
    </item>
  </channel>
</rss>