<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX53 uboot issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX53-uboot-issue/m-p/398315#M58512</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with a custom board based on the MX53QSB (MCIMX53-START-R). The only difference is the USB OTG has been omitted. The custom board boots fine with the MCIMX535-START-R-BSP-11-09_C image, but the core-image-minimal build from yocto (using the IMX53QSB machine on Daisy) does not boot. The following is output when trying to boot from the core-image-minimal build:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"U-Boot 2013.10 (Sep 17 2015 - 15:22:06)&lt;/P&gt;&lt;P&gt;Board: MX53 LOCO&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp; 1 GiB&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;MMC: no card present&lt;BR /&gt;MMC init failed&lt;BR /&gt;Using default environment&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX53 family rev2.1 at 1000 MHz&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; FEC&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;BR /&gt;MMC: no card present&lt;BR /&gt;mmc0(part 0) is current device&lt;BR /&gt;MMC: no card present"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It appears that the yocto uboot build doesn't see the SDcard. I used the MCIMX535-START-R-BSP-11-09_C image to check the fuse settings on the MCIMX53-START-R board and burnt the same fuses on the custom board. I've used the OBDS tools in the MCIMX535-START-R-BSP-11-09_C image to test out the peripherals, and everything seems to be operational hardware wise. Does anyone have any insight as to why the yocto uboot isn't seeing the sdcard?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Sep 2015 14:43:11 GMT</pubDate>
    <dc:creator>mackwarren</dc:creator>
    <dc:date>2015-09-21T14:43:11Z</dc:date>
    <item>
      <title>IMX53 uboot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX53-uboot-issue/m-p/398315#M58512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with a custom board based on the MX53QSB (MCIMX53-START-R). The only difference is the USB OTG has been omitted. The custom board boots fine with the MCIMX535-START-R-BSP-11-09_C image, but the core-image-minimal build from yocto (using the IMX53QSB machine on Daisy) does not boot. The following is output when trying to boot from the core-image-minimal build:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"U-Boot 2013.10 (Sep 17 2015 - 15:22:06)&lt;/P&gt;&lt;P&gt;Board: MX53 LOCO&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp; 1 GiB&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;MMC: no card present&lt;BR /&gt;MMC init failed&lt;BR /&gt;Using default environment&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX53 family rev2.1 at 1000 MHz&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; FEC&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;BR /&gt;MMC: no card present&lt;BR /&gt;mmc0(part 0) is current device&lt;BR /&gt;MMC: no card present"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It appears that the yocto uboot build doesn't see the SDcard. I used the MCIMX535-START-R-BSP-11-09_C image to check the fuse settings on the MCIMX53-START-R board and burnt the same fuses on the custom board. I've used the OBDS tools in the MCIMX535-START-R-BSP-11-09_C image to test out the peripherals, and everything seems to be operational hardware wise. Does anyone have any insight as to why the yocto uboot isn't seeing the sdcard?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Sep 2015 14:43:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX53-uboot-issue/m-p/398315#M58512</guid>
      <dc:creator>mackwarren</dc:creator>
      <dc:date>2015-09-21T14:43:11Z</dc:date>
    </item>
    <item>
      <title>Re: IMX53 uboot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX53-uboot-issue/m-p/398316#M58513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mack&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check SDcard cd signal and check iomux settings for image,&lt;/P&gt;&lt;P&gt;sect.1.3.3 Adding New Driver Initialization Code to Board Files attached Porting&lt;/P&gt;&lt;P&gt;Guide describes uboot modifications. Just for test one can try with uboot from&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Linux 2.6.35 Source Code Files and documentation 11.09.&lt;/P&gt;&lt;P&gt;Supports MCIMX53-START and MCIMX53-START-R (REV 2011.09)&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx53-processors/i.mx53-quick-start-board:IMX53QSB?fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx53-processors/i.mx53-quick-start-board:IMX53QSB?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx53-processors/i.mx5…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 04:15:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX53-uboot-issue/m-p/398316#M58513</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-22T04:15:52Z</dc:date>
    </item>
  </channel>
</rss>