<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SPI without MISO in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPI-without-MISO/m-p/398227#M58502</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Instead of building an SPI port with MOSI and MISO lanes, is it possible to have two symmetric seperate SPI interface with only MOSI lanes between i.MX6 and an FPGA?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Apr 2015 14:20:35 GMT</pubDate>
    <dc:creator>mustafademirci</dc:creator>
    <dc:date>2015-04-10T14:20:35Z</dc:date>
    <item>
      <title>SPI without MISO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-without-MISO/m-p/398227#M58502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Instead of building an SPI port with MOSI and MISO lanes, is it possible to have two symmetric seperate SPI interface with only MOSI lanes between i.MX6 and an FPGA?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2015 14:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-without-MISO/m-p/398227#M58502</guid>
      <dc:creator>mustafademirci</dc:creator>
      <dc:date>2015-04-10T14:20:35Z</dc:date>
    </item>
    <item>
      <title>Re: SPI without MISO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-without-MISO/m-p/398228#M58503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Mustafa&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems one can use configuration with&lt;/P&gt;&lt;P&gt;one interface as master, other slave.&amp;nbsp; One can look at&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt;&amp;nbsp; sect.21.1.2 Modes and Operations&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Apr 2015 00:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-without-MISO/m-p/398228#M58503</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-11T00:57:11Z</dc:date>
    </item>
  </channel>
</rss>