<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6 Sabre Auto DL: Using ECSPI and USB Simultaneously in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Sabre-Auto-DL-Using-ECSPI-and-USB-Simultaneously/m-p/397518#M58367</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an interesting puzzle here. In the imx6dl-sabreauto-ecspi.dts, turning on ecspi requires turning off usbh1 because i2c3 has a pin conflict with ecspi. I was curious if there was any way to reroute the i2c configuration so that both usb and ecspi can be used simultaneously. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the schematic it appears MAX7310_b can be controlled by i2c2 or i2c3. Since i2c3 has the pin conflict how would I migrate over the dts and dtsi code to i2c2? Or is that even possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jonathon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Aug 2015 18:59:27 GMT</pubDate>
    <dc:creator>jonathon_reach</dc:creator>
    <dc:date>2015-08-25T18:59:27Z</dc:date>
    <item>
      <title>iMX6 Sabre Auto DL: Using ECSPI and USB Simultaneously</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Sabre-Auto-DL-Using-ECSPI-and-USB-Simultaneously/m-p/397518#M58367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an interesting puzzle here. In the imx6dl-sabreauto-ecspi.dts, turning on ecspi requires turning off usbh1 because i2c3 has a pin conflict with ecspi. I was curious if there was any way to reroute the i2c configuration so that both usb and ecspi can be used simultaneously. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the schematic it appears MAX7310_b can be controlled by i2c2 or i2c3. Since i2c3 has the pin conflict how would I migrate over the dts and dtsi code to i2c2? Or is that even possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jonathon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Aug 2015 18:59:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Sabre-Auto-DL-Using-ECSPI-and-USB-Simultaneously/m-p/397518#M58367</guid>
      <dc:creator>jonathon_reach</dc:creator>
      <dc:date>2015-08-25T18:59:27Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Sabre Auto DL: Using ECSPI and USB Simultaneously</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Sabre-Auto-DL-Using-ECSPI-and-USB-Simultaneously/m-p/397519#M58368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It should be possible to use the I2C_2 module instead. But as you can see in the below image the R713 and R689 resistors are not populated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55807iA3E33AE8A8A326DD/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You would have to place them and to avoid any conflict remove R84 and R64.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Sep 2015 22:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Sabre-Auto-DL-Using-ECSPI-and-USB-Simultaneously/m-p/397519#M58368</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-09-10T22:17:00Z</dc:date>
    </item>
  </channel>
</rss>