<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6Q: Maximum IPU clock frequency</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Maximum-IPU-clock-frequency/m-p/396885#M58232</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the maximum clock frequency for the IPU clock in IMX6Q? According to reference manual it is 264 MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But in this answer: &lt;A href="https://community.nxp.com/docs/DOC-98282"&gt;Q&amp;amp;amp;A: What are the maximum HSP_CLK frequency values?&lt;/A&gt; it says "&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;IPU1_HSP_CLK_ROOT is 270 MHz for DQ" but then writes max for DQ is 264 MHz. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;The only way to achieve 264 MHz is to divide MMDC_CH0_AXI_CLK_ROOT. But I'm using LPDDR2 memory rated at 400 MHz and I'm running MMDC at 396 MHz so that is not an option.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;270 MHz is achievable by selecting PLL3_PFD1 at 540 MHz and dividing by 2. I have tested this and it seems to work fine but it's unclear if this is a supported frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If 270 MHz is not guaranteed to work, the clock options for the IPUs seems quite strange. I can only get 270 MHz, 198 MHz or lower if I'm running the memory at 400 MHz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Sep 2015 11:58:07 GMT</pubDate>
    <dc:creator>kristofferglemb</dc:creator>
    <dc:date>2015-09-21T11:58:07Z</dc:date>
    <item>
      <title>IMX6Q: Maximum IPU clock frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Maximum-IPU-clock-frequency/m-p/396885#M58232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the maximum clock frequency for the IPU clock in IMX6Q? According to reference manual it is 264 MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But in this answer: &lt;A href="https://community.nxp.com/docs/DOC-98282"&gt;Q&amp;amp;amp;A: What are the maximum HSP_CLK frequency values?&lt;/A&gt; it says "&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;IPU1_HSP_CLK_ROOT is 270 MHz for DQ" but then writes max for DQ is 264 MHz. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;The only way to achieve 264 MHz is to divide MMDC_CH0_AXI_CLK_ROOT. But I'm using LPDDR2 memory rated at 400 MHz and I'm running MMDC at 396 MHz so that is not an option.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;270 MHz is achievable by selecting PLL3_PFD1 at 540 MHz and dividing by 2. I have tested this and it seems to work fine but it's unclear if this is a supported frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If 270 MHz is not guaranteed to work, the clock options for the IPUs seems quite strange. I can only get 270 MHz, 198 MHz or lower if I'm running the memory at 400 MHz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Sep 2015 11:58:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Maximum-IPU-clock-frequency/m-p/396885#M58232</guid>
      <dc:creator>kristofferglemb</dc:creator>
      <dc:date>2015-09-21T11:58:07Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q: Maximum IPU clock frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Maximum-IPU-clock-frequency/m-p/396886#M58233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is possible to use 270MHz clock, derived from the PLL3 PFD1, as the IPU main clock.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 08:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Maximum-IPU-clock-frequency/m-p/396886#M58233</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-09-22T08:25:03Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q: Maximum IPU clock frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Maximum-IPU-clock-frequency/m-p/396887#M58234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's great, but it really begs the question why the reference manual and QA claims 264 MHz?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 12:41:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Maximum-IPU-clock-frequency/m-p/396887#M58234</guid>
      <dc:creator>kristofferglemb</dc:creator>
      <dc:date>2015-09-22T12:41:46Z</dc:date>
    </item>
  </channel>
</rss>