<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 使用KSZ9031 IC，Ethernet 无法使用1000M Lan in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/%E4%BD%BF%E7%94%A8KSZ9031-IC-Ethernet-%E6%97%A0%E6%B3%95%E4%BD%BF%E7%94%A81000M-Lan/m-p/396825#M58223</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi :&lt;SPAN class="font-color-meta" style="padding: 0 0 5px; font-size: 1.2em; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #9aa9af; background-color: #e6e6e6;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works now,thanks!&lt;/P&gt;&lt;P&gt;But there is another problem. As we know,IMX6DL ethernet's max speed is 400M,but we can only reach 200M,is there other registers we should adjust?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Leo GUo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 May 2015 00:46:30 GMT</pubDate>
    <dc:creator>daqiang</dc:creator>
    <dc:date>2015-05-29T00:46:30Z</dc:date>
    <item>
      <title>使用KSZ9031 IC，Ethernet 无法使用1000M Lan</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/%E4%BD%BF%E7%94%A8KSZ9031-IC-Ethernet-%E6%97%A0%E6%B3%95%E4%BD%BF%E7%94%A81000M-Lan/m-p/396823#M58221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;我们使用的是KSZ9031方案，如果设置成10M/100M都没问题，但如果设置成1000M，则无法连接。&lt;/P&gt;&lt;P&gt;路由器是支持1000M的。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2015 11:24:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/%E4%BD%BF%E7%94%A8KSZ9031-IC-Ethernet-%E6%97%A0%E6%B3%95%E4%BD%BF%E7%94%A81000M-Lan/m-p/396823#M58221</guid>
      <dc:creator>daqiang</dc:creator>
      <dc:date>2015-05-26T11:24:00Z</dc:date>
    </item>
    <item>
      <title>Re: 使用KSZ9031 IC，Ethernet 无法使用1000M Lan</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/%E4%BD%BF%E7%94%A8KSZ9031-IC-Ethernet-%E6%97%A0%E6%B3%95%E4%BD%BF%E7%94%A81000M-Lan/m-p/396824#M58222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Translated by Google:&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;Use&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;KSZ9031 IC, Ethernet&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;can not use the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;1000M Lan&lt;/SPAN&gt;&lt;BR /&gt; &lt;SPAN class="hps"&gt;We are using&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;KSZ9031&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;scenario, if&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;set to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;10M / 100M&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;no problem,&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;but&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;if&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;set to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;1000M,&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;you can not connect&lt;/SPAN&gt;.&lt;BR /&gt; &lt;SPAN class="hps"&gt;Router&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;supports&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the 1000M&lt;/SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi Guo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;suggest to check Table 62. RGMII Signal Switching Specifications &lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQCEC&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and configure KSZ9031 registers if necessary, like&lt;/P&gt;&lt;P&gt;MMD Address 2h&amp;nbsp; Register 5h - RGMII RX Data Pad Skew&lt;/P&gt;&lt;P&gt;MMD Address 2h&amp;nbsp; Register 6h - RGMII TX Data Pad Skew&lt;/P&gt;&lt;P&gt;MMD Address 2h&amp;nbsp; Register 8h - RGMII Clock Pad Skew&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note, for i.MX6 ENET there is no control on-chip to adjust the delay between &lt;/P&gt;&lt;P&gt;these signals. A delay would need to be implemented at the board level.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2015 09:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/%E4%BD%BF%E7%94%A8KSZ9031-IC-Ethernet-%E6%97%A0%E6%B3%95%E4%BD%BF%E7%94%A81000M-Lan/m-p/396824#M58222</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-05-27T09:16:18Z</dc:date>
    </item>
    <item>
      <title>Re: 使用KSZ9031 IC，Ethernet 无法使用1000M Lan</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/%E4%BD%BF%E7%94%A8KSZ9031-IC-Ethernet-%E6%97%A0%E6%B3%95%E4%BD%BF%E7%94%A81000M-Lan/m-p/396825#M58223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi :&lt;SPAN class="font-color-meta" style="padding: 0 0 5px; font-size: 1.2em; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #9aa9af; background-color: #e6e6e6;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works now,thanks!&lt;/P&gt;&lt;P&gt;But there is another problem. As we know,IMX6DL ethernet's max speed is 400M,but we can only reach 200M,is there other registers we should adjust?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Leo GUo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2015 00:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/%E4%BD%BF%E7%94%A8KSZ9031-IC-Ethernet-%E6%97%A0%E6%B3%95%E4%BD%BF%E7%94%A81000M-Lan/m-p/396825#M58223</guid>
      <dc:creator>daqiang</dc:creator>
      <dc:date>2015-05-29T00:46:30Z</dc:date>
    </item>
    <item>
      <title>Re: 使用KSZ9031 IC，Ethernet 无法使用1000M Lan</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/%E4%BD%BF%E7%94%A8KSZ9031-IC-Ethernet-%E6%97%A0%E6%B3%95%E4%BD%BF%E7%94%A81000M-Lan/m-p/396826#M58224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;请问是怎么修复的呢，千兆不可用的情况&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2020 09:20:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/%E4%BD%BF%E7%94%A8KSZ9031-IC-Ethernet-%E6%97%A0%E6%B3%95%E4%BD%BF%E7%94%A81000M-Lan/m-p/396826#M58224</guid>
      <dc:creator>chenw</dc:creator>
      <dc:date>2020-08-07T09:20:16Z</dc:date>
    </item>
  </channel>
</rss>