<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Question, MC34704 VIN current</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-MC34704-VIN-current/m-p/396695#M58191</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a customer who is using MC34704 with i.MX25.&lt;/P&gt;&lt;P&gt;And 5V is supplied into VIN of MC34704, and REG2,3,4 are used on his board.&lt;/P&gt;&lt;P&gt;In that case, where can I find the description which can be helpful to estimate the current flowing into PVIN2,3,4(VIN)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Aug 2015 03:10:55 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2015-08-26T03:10:55Z</dc:date>
    <item>
      <title>Question, MC34704 VIN current</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-MC34704-VIN-current/m-p/396695#M58191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a customer who is using MC34704 with i.MX25.&lt;/P&gt;&lt;P&gt;And 5V is supplied into VIN of MC34704, and REG2,3,4 are used on his board.&lt;/P&gt;&lt;P&gt;In that case, where can I find the description which can be helpful to estimate the current flowing into PVIN2,3,4(VIN)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2015 03:10:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-MC34704-VIN-current/m-p/396695#M58191</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-08-26T03:10:55Z</dc:date>
    </item>
    <item>
      <title>Re: Question, MC34704 VIN current</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-MC34704-VIN-current/m-p/396696#M58192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The estimation is quite simple in that case. Let's consider it on "per regulator" basis.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. First, calculate the power that the regulator 'x' provides to a load: Pout_x = Vout_x * Iout_x, where Pout_x is the output power of a regulator 'x', Vout_x and Iout_x - its output voltage and current, respectively.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Then, assuming the typical conversion efficiency of regulator as 80% (denoted in the data sheet), multiply the Pout_x by 1.25 (1/0.8) to calculate the power that the regulator 'x' consumes on its input: Pin_x = Pout_x *1.25 .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. Now, knowing the input power and input voltage, we can calculate the input current: Iin_x = Pin_x / Vin_x .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming the input voltage of 5V, the final calculation for a regulator 'x' is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Iin_x = (Vout_x * Iout_x * 1.25) / 5 = (Vout_x * Iout_x) / 4 .&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Aug 2015 08:56:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-MC34704-VIN-current/m-p/396696#M58192</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-08-27T08:56:40Z</dc:date>
    </item>
  </channel>
</rss>