<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How many camera inputs can be used in IMX6 Quad simultaneously? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-many-camera-inputs-can-be-used-in-IMX6-Quad-simultaneously/m-p/396336#M58105</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX6Quad processor has three camera ports, physically routed out of the chip: two parallel ones (IPU1_CSI0 and IPU2_CSI1) and one MIPI CSI. The MIPI CSI port input can be routed to any of the two IPUs with so-called MIPI_CSI-to-IPU gasket module. And, yes, you can use all these three ports simultaneously.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Jul 2015 06:35:13 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2015-07-30T06:35:13Z</dc:date>
    <item>
      <title>How many camera inputs can be used in IMX6 Quad simultaneously?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-many-camera-inputs-can-be-used-in-IMX6-Quad-simultaneously/m-p/396334#M58103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now using IMX6 Quad.&lt;/P&gt;&lt;P&gt;I know it support 2 parallel ports and 1 MIPI port.&lt;/P&gt;&lt;P&gt;IMX6 Quad has 2 IPUs.&lt;/P&gt;&lt;P&gt;Could you please tell me can it use these 3 ports simultaneously?&lt;/P&gt;&lt;P&gt;If it can, is it right that&amp;nbsp; MIPI and 1 parallel use 1 IPU and the other parallel use another IPU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ivy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2015 00:04:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-many-camera-inputs-can-be-used-in-IMX6-Quad-simultaneously/m-p/396334#M58103</guid>
      <dc:creator>ivyliu</dc:creator>
      <dc:date>2015-07-30T00:04:40Z</dc:date>
    </item>
    <item>
      <title>Re: How many camera inputs can be used in IMX6 Quad simultaneously?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-many-camera-inputs-can-be-used-in-IMX6-Quad-simultaneously/m-p/396335#M58104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ivy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right: two IPUs and each has two CSI :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53546iBC0AEFAA844928C9/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In general you can connect 4 cameras to the MIPI CSI-2 interface.&lt;/P&gt;&lt;P&gt;For this you have to multiplex the four streams in an FPGA. &lt;/P&gt;&lt;P&gt;Each camera in this case should use a different stream &lt;/P&gt;&lt;P&gt;identifier (stream 0-3),&amp;nbsp; 4 data streams can the be distributed across &lt;/P&gt;&lt;P&gt;the 4 CSI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2015 01:53:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-many-camera-inputs-can-be-used-in-IMX6-Quad-simultaneously/m-p/396335#M58104</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-30T01:53:27Z</dc:date>
    </item>
    <item>
      <title>Re: How many camera inputs can be used in IMX6 Quad simultaneously?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-many-camera-inputs-can-be-used-in-IMX6-Quad-simultaneously/m-p/396336#M58105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX6Quad processor has three camera ports, physically routed out of the chip: two parallel ones (IPU1_CSI0 and IPU2_CSI1) and one MIPI CSI. The MIPI CSI port input can be routed to any of the two IPUs with so-called MIPI_CSI-to-IPU gasket module. And, yes, you can use all these three ports simultaneously.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2015 06:35:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-many-camera-inputs-can-be-used-in-IMX6-Quad-simultaneously/m-p/396336#M58105</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-07-30T06:35:13Z</dc:date>
    </item>
    <item>
      <title>Re: How many camera inputs can be used in IMX6 Quad simultaneously?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-many-camera-inputs-can-be-used-in-IMX6-Quad-simultaneously/m-p/396337#M58106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor and Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for the prompt reply!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ivy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2015 15:12:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-many-camera-inputs-can-be-used-in-IMX6-Quad-simultaneously/m-p/396337#M58106</guid>
      <dc:creator>ivyliu</dc:creator>
      <dc:date>2015-07-30T15:12:45Z</dc:date>
    </item>
    <item>
      <title>Re: How many camera inputs can be used in IMX6 Quad simultaneously?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-many-camera-inputs-can-be-used-in-IMX6-Quad-simultaneously/m-p/396338#M58107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your prompt reply!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ivy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2015 16:30:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-many-camera-inputs-can-be-used-in-IMX6-Quad-simultaneously/m-p/396338#M58107</guid>
      <dc:creator>ivyliu</dc:creator>
      <dc:date>2015-08-20T16:30:14Z</dc:date>
    </item>
  </channel>
</rss>