<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: U-boot customization for customized board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-customization-for-customized-board/m-p/396252#M58095</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Srinivasa&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ccm-&amp;gt;CCGRx define whch modules are used ("1" in CCGRx) in uboot, which&lt;/P&gt;&lt;P&gt;not. Description can be found in CCM chapter of RM.&lt;/P&gt;&lt;P&gt;Regarding mx6_ddr_sysinfo, one can look at presentation with&lt;/P&gt;&lt;P&gt;description MMDC settings&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="1470" data-containertype="600" data-objectid="104363" data-objecttype="102" href="https://community.freescale.com/docs/DOC-104363"&gt;https://community.freescale.com/docs/DOC-104363&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Oct 2015 08:40:19 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-10-14T08:40:19Z</dc:date>
    <item>
      <title>U-boot customization for customized board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-customization-for-customized-board/m-p/396251#M58094</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have got customized board based on IMX6D. Now, we are bringing up the board for which we are customizing U-Boot and compiling it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, for some of the freescale boards ccgr_init() is like below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static void ccgr_init(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; struct mxc_ccm_reg *ccm = (struct mxc_ccm_reg *)CCM_BASE_ADDR;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0xFFFFFFFF, &amp;amp;ccm-&amp;gt;CCGR0);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0xFFFFFFFF, &amp;amp;ccm-&amp;gt;CCGR1);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0xFFFFFFFF, &amp;amp;ccm-&amp;gt;CCGR2);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0xFFFFFFFF, &amp;amp;ccm-&amp;gt;CCGR3);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0xFFFFFFFF, &amp;amp;ccm-&amp;gt;CCGR4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0xFFFFFFFF, &amp;amp;ccm-&amp;gt;CCGR5);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0xFFFFFFFF, &amp;amp;ccm-&amp;gt;CCGR6);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0x00260324, &amp;amp;ccm-&amp;gt;cbcmr);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;where as some of the boards ccgr_init() function is defined as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static void ccgr_init(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; struct mxc_ccm_reg *ccm = (struct mxc_ccm_reg *)CCM_BASE_ADDR;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0x00C03F3F, &amp;amp;ccm-&amp;gt;CCGR0);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0x0030FC03, &amp;amp;ccm-&amp;gt;CCGR1);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0x0FFFC000, &amp;amp;ccm-&amp;gt;CCGR2);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0x3FF00000, &amp;amp;ccm-&amp;gt;CCGR3);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0x00FFF300, &amp;amp;ccm-&amp;gt;CCGR4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0x0F0000C3, &amp;amp;ccm-&amp;gt;CCGR5);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(0x000003FF, &amp;amp;ccm-&amp;gt;CCGR6);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how to write ccgr_init() function for our board. how to arrive at those values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also, i have another query on&amp;nbsp; mx6_ddr_sysinfo () (from imx_ddr.h)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;struct mx6_ddr_sysinfo {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8 dsize;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* size of bus (in dwords: 0=16bit,1=32bit,2=64bit) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8 cs_density;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* density per chip select (Gb) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8 ncs;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* number chip selects used (1|2) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; char cs1_mirror;/* enable address mirror (0|1) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; char bi_on;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Bank interleaving enable */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8 rtt_nom;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Rtt_Nom (DDR3_RTT_*) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8 rtt_wr;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Rtt_Wr (DDR3_RTT_*) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8 ralat;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Read Additional Latency (0-7) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8 walat;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Write Additional Latency (0-3) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8 mif3_mode;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Command prediction working mode */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8 rst_to_cke;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Time from SDE enable to CKE rise */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8 sde_to_rst;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Time from SDE enable until DDR reset# is high */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8 pd_fast_exit;/* enable precharge powerdown fast-exit */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; u8 ddr_type;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* DDR type: DDR3(0) or LPDDR2(1) */&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; in this .cs-density value should be given as 2 if our DDR is 2Gb per chip select. But some places like Sabresd they are using 24, and some places they are using 20 etc.&amp;nbsp; how to get correct value.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 05:56:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-boot-customization-for-customized-board/m-p/396251#M58094</guid>
      <dc:creator>srinivasaporam</dc:creator>
      <dc:date>2015-10-14T05:56:26Z</dc:date>
    </item>
    <item>
      <title>Re: U-boot customization for customized board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-customization-for-customized-board/m-p/396252#M58095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Srinivasa&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ccm-&amp;gt;CCGRx define whch modules are used ("1" in CCGRx) in uboot, which&lt;/P&gt;&lt;P&gt;not. Description can be found in CCM chapter of RM.&lt;/P&gt;&lt;P&gt;Regarding mx6_ddr_sysinfo, one can look at presentation with&lt;/P&gt;&lt;P&gt;description MMDC settings&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="1470" data-containertype="600" data-objectid="104363" data-objecttype="102" href="https://community.freescale.com/docs/DOC-104363"&gt;https://community.freescale.com/docs/DOC-104363&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 08:40:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-boot-customization-for-customized-board/m-p/396252#M58095</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-10-14T08:40:19Z</dc:date>
    </item>
  </channel>
</rss>