<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Hardware Trigger for Image Capture in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Hardware-Trigger-for-Image-Capture/m-p/395922#M58035</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raja&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to use for such purpose CSIx_DATA_EN.&lt;/P&gt;&lt;P&gt;Also as sensor is master for synchronization signals, it can&lt;/P&gt;&lt;P&gt;provide ability for external sync. One can consult with sensor datasheet&lt;/P&gt;&lt;P&gt;for availability of such feature.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Sep 2015 07:39:34 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-09-21T07:39:34Z</dc:date>
    <item>
      <title>Hardware Trigger for Image Capture</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hardware-Trigger-for-Image-Capture/m-p/395921#M58034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the example codes provided for image capture from OV5640 using imx6, i always see that the image capture is using v4l2 either being read from a older buffer or started with a software trigger. Is it possible to start a image capture using external hardware trigger? is there any driver or v4l2 limitation? is there a feature in ov5640 that can be used to achieve this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want the frame at a particular instant where the hardware trigger is happening. So it is not possible to start a capture from software in my application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Sep 2015 05:20:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hardware-Trigger-for-Image-Capture/m-p/395921#M58034</guid>
      <dc:creator>rajabalaji</dc:creator>
      <dc:date>2015-09-21T05:20:51Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware Trigger for Image Capture</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hardware-Trigger-for-Image-Capture/m-p/395922#M58035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raja&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to use for such purpose CSIx_DATA_EN.&lt;/P&gt;&lt;P&gt;Also as sensor is master for synchronization signals, it can&lt;/P&gt;&lt;P&gt;provide ability for external sync. One can consult with sensor datasheet&lt;/P&gt;&lt;P&gt;for availability of such feature.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Sep 2015 07:39:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hardware-Trigger-for-Image-Capture/m-p/395922#M58035</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-21T07:39:34Z</dc:date>
    </item>
  </channel>
</rss>