<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic U-Boot booting off parallel NOR on ARD in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-booting-off-parallel-NOR-on-ARD/m-p/172132#M5775</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Howdy&lt;/P&gt;&lt;P&gt;Anybody tried to build and boot U-Boot off the ARD board's parallel NOR flash. I'm using a DDR3 Automotive board not a Tablet but thought it would be similar.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Long story short, setting up the IVT should be as simple as setting the correct offset but the plug-in has hard-coded offset for the SD card so I know it was probably never tested in that configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also any help with setting up the IVT/Boot Data Structure for run in place on the NOR would be appreciated. Should I still use the ROM plug-in hooks to init the DDR or just copy the code into into "start" and be done with it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Switched over to the OBDS because it has the IVT and U-Boot failed to compile when I commited out the CONFIG_SYS_NO_FLASH which forces U-Boot to init the NOR flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Jul 2012 16:28:49 GMT</pubDate>
    <dc:creator>RSmith</dc:creator>
    <dc:date>2012-07-02T16:28:49Z</dc:date>
    <item>
      <title>U-Boot booting off parallel NOR on ARD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-booting-off-parallel-NOR-on-ARD/m-p/172132#M5775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Howdy&lt;/P&gt;&lt;P&gt;Anybody tried to build and boot U-Boot off the ARD board's parallel NOR flash. I'm using a DDR3 Automotive board not a Tablet but thought it would be similar.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Long story short, setting up the IVT should be as simple as setting the correct offset but the plug-in has hard-coded offset for the SD card so I know it was probably never tested in that configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also any help with setting up the IVT/Boot Data Structure for run in place on the NOR would be appreciated. Should I still use the ROM plug-in hooks to init the DDR or just copy the code into into "start" and be done with it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Switched over to the OBDS because it has the IVT and U-Boot failed to compile when I commited out the CONFIG_SYS_NO_FLASH which forces U-Boot to init the NOR flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jul 2012 16:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-booting-off-parallel-NOR-on-ARD/m-p/172132#M5775</guid>
      <dc:creator>RSmith</dc:creator>
      <dc:date>2012-07-02T16:28:49Z</dc:date>
    </item>
  </channel>
</rss>