<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX233 NAND in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-NAND/m-p/394105#M57625</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;i followed the istruction of User Guide for i.MX28 On-Board Diagnostics Suite (OBDS) for build a mx28-obds.sb file and flashed it on sd, but when boot a message appear on console &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Undefined Instruction&lt;/P&gt;&lt;P&gt;r14_un&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i tried to usb boot using sb_loader with the same results&lt;/P&gt;&lt;P&gt;after this i edited the build_mx28.sh script to chagne the elftosb option from "-f mx28" to "-f mx23" but at the end of building an error message say:&lt;/P&gt;&lt;P&gt;error: line 20: HAB features not supported with the selected family&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Oct 2015 19:09:41 GMT</pubDate>
    <dc:creator>federicodevitii</dc:creator>
    <dc:date>2015-10-14T19:09:41Z</dc:date>
    <item>
      <title>i.MX233 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-NAND/m-p/394103#M57623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i've build a i.Mx233 (128-QFP) based board with a 29F8G08ABABA NAND. I connected&amp;nbsp; GPMI_CLE, GPMI_ALE, GPMI_CE0# (pulled up via 47k resistor), GPMI_RE#, GPMI_WE#, GPMI_WP# (pulled down via 47k resistor), GPMI_R/B0# (pulled up via 47k resistor) from soc to nand, and on the nand i connected VSS1&amp;amp;VSS2 to gnd and VCC1&amp;amp;VCC2 to 3v3.&lt;/P&gt;&lt;P&gt;When i try write the flash via mfgtools, the nand is not recognized.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PowerPrep start initialize power...&lt;/P&gt;&lt;P&gt;Battery Voltage = 0.80V&lt;/P&gt;&lt;P&gt;No battery or bad battery&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; detected!!!.Disabling battery&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; voltage measurements./r/nLLCJul&amp;nbsp; 1 201017:35:57&lt;/P&gt;&lt;P&gt;EMI_CTRL 0x1C084040&lt;/P&gt;&lt;P&gt;FRAC 0x92926152&lt;/P&gt;&lt;P&gt;init_ddr_mt46v32m16_133Mhz&lt;/P&gt;&lt;P&gt;power 0x00820710&lt;/P&gt;&lt;P&gt;Frac 0x92926152&lt;/P&gt;&lt;P&gt;start change cpu freq&lt;/P&gt;&lt;P&gt;hbus 0x00000003&lt;/P&gt;&lt;P&gt;cpu 0x00010002&lt;/P&gt;&lt;P&gt;LLLLLLLFCLFLJUncompressing Linux...................................................................................... done, booting the kernel.&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Linux version 2.6.31-680-g9eb6b19-updater-00015-ga63ad47-dirty (b29397@shlinux1) (gcc version 4.1.2) #1 PREEMPT Thu Jul 1 17:21:44 CST 2010&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] CPU: VIVT data cache, VIVT instruction cache&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Machine: Freescale MX23EVK board&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Memory policy: ECC disabled, Data cache writeback&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 16256&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Kernel command line: console=ttyAM0,115200 rdinit=/linuxrc rw gpmi&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] PID hash table entries: 256 (order: 8, 1024 bytes)&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Memory: 64MB = 64MB total&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Memory: 57964KB available (2368K code, 271K data, 96K init, 0K highmem)&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] NR_IRQS:224&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Console: colour dummy device 80x30&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] console [ttyAM0] enabled&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.010000] Calibrating delay loop... 115.91 BogoMIPS (lpj=579584)&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.230000] Mount-cache hash table entries: 512&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.230000] CPU: Testing write buffer coherency: ok&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.250000] regulator: core version 0.5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.270000] regulator: vddd: 800 &amp;lt;--&amp;gt; 1575 mV fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.270000] regulator: vddd_bo: 800 &amp;lt;--&amp;gt; 1575 mV fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.280000] regulator: vdda: 1500 &amp;lt;--&amp;gt; 2275 mV fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.280000] regulator: vddio: 2800 &amp;lt;--&amp;gt; 3575 mV fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.290000] regulator: overall_current: 0 &amp;lt;--&amp;gt; 2147483 mA fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.290000] regulator: mxs-duart-1: 0 &amp;lt;--&amp;gt; 2147483 mA fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.300000] regulator: mxs-bl-1: 0 &amp;lt;--&amp;gt; 2147483 mA fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.300000] regulator: mxs-i2c-1: 0 &amp;lt;--&amp;gt; 2147483 mA fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.310000] regulator: mmc_ssp-1: 0 &amp;lt;--&amp;gt; 2147483 mA fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.310000] regulator: mmc_ssp-2: 0 &amp;lt;--&amp;gt; 2147483 mA fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.320000] regulator: charger-1: 0 &amp;lt;--&amp;gt; 2147483 mA fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.320000] regulator: power-test-1: 0 &amp;lt;--&amp;gt; 2147483 mA fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.330000] regulator: cpufreq-1: 0 &amp;lt;--&amp;gt; 2147483 mA fast normal&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.340000] i.MX IRAM pool: 28 KB@0xc4808000&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.370000] bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.380000] usbcore: registered new interface driver usbfs&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.380000] usbcore: registered new interface driver hub&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.390000] usbcore: registered new device driver usb&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.410000] Trying to unpack rootfs image as initramfs...&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.180000] Freeing initrd memory: 4096K&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.190000] Bus freq driver module loaded&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.190000] usb: DR gadget (utmi) registered&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.210000] mxs_cpu_init: cpufreq init finished&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.220000] JFFS2 version 2.2. (NAND) (SUMMARY)&amp;nbsp; © 2001-2006 Red Hat, Inc.&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.230000] msgmni has been set to 121&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.250000] io scheduler noop registered&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.250000] io scheduler anticipatory registered&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.260000] io scheduler deadline registered&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.260000] io scheduler cfq registered (default)&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.660000] Console: switching to colour frame buffer device 60x34&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.940000] mxs-duart.0: ttyAM0 at MMIO 0x80070000 (irq = 0) is a DebugUART&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.950000] mxs-auart.1: ttySP1 at MMIO 0x8006c000 (irq = 24) is a mxs-auart.1&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.960000] Found APPUART 3.0.0&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.990000] brd: module loaded&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.000000] i.MX GPMI NFC&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.000000] NFC: Version 0, 4-chip GPMI and BCH&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.010000] Boot ROM: Version 0, Single/dual-chip boot area, no block mark swapping&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.010000] Scanning for NAND Flash chips...&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d;"&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.020000] No NAND device found!!!&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.020000] gpmi-nfc gpmi-nfc.0: Chip scan failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.030000] ARC USBOTG Device Controller driver (1 August 2005)&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.060000] check_parameters:UTP settings are in place now, overriding defaults&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.060000] g_file_storage gadget: File-backed Storage Gadget, version: 20 November 2008&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.070000] g_file_storage gadget: Number of LUNs=1&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.180000] udc run&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.180000] fsl-usb2-udc: bind to driver g_file_storage&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.190000] MXS RTC driver v1.0 hardware v2.0.0&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.190000] mxs-rtc mxs-rtc.0: rtc core: registered mxs-rtc as rtc0&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.200000] mxs-mmc: MXS SSP Controller MMC Interface driver&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.310000] mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 14 ERRIRQ 15&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.320000] mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:19:02 UTC (1142)&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.320000] Freeing init memory: 96K&lt;/P&gt;&lt;P&gt;Starting UTP&lt;/P&gt;&lt;P&gt;disable turn off display&lt;/P&gt;&lt;P&gt;uuc 0.4 [built Jul&amp;nbsp; 1 2010 16:13:58]&lt;/P&gt;&lt;P&gt;UTP: Waiting for device to appear&lt;/P&gt;&lt;P&gt;utp_mk_devnode: creating node '/dev/utp' with 10+222&lt;/P&gt;&lt;P&gt;The watchdog is not configured, needed by mx35/mx51/mx53&lt;/P&gt;&lt;P&gt;658, No such device&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 5.060000] g_file_storage gadget: high speed config #1&lt;/P&gt;&lt;P&gt;UTP: received command 'm[&amp;nbsp;&amp;nbsp;&amp;nbsp; 6.580000] utp_exec: exit with status -22&lt;/P&gt;&lt;P&gt;knod class/mtd,mtd0,/dev/mtd0'&lt;/P&gt;&lt;P&gt;class = 'class/mtd'&lt;/P&gt;&lt;P&gt;item = 'mtd0'&lt;/P&gt;&lt;P&gt;node = /dev/mtd0&lt;/P&gt;&lt;P&gt;type = (null)&lt;/P&gt;&lt;P&gt;UTP: running utp_mk_devnode(class/mtd,mtd0,/dev/mtd0,0x2000)&lt;/P&gt;&lt;P&gt;UTP: sending Non-success&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;whats' wrong?&lt;/P&gt;&lt;P&gt;i wrote via bitburner in the HW_OCOTP_ROM1 register&amp;nbsp; the bit NUMBER_OF_NAND to1 and ENABLE_NAND0_CE_RDY_PULLUP to blown (it's redundant with the pull-up resistor, i know)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can someone help me, please&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Oct 2015 19:24:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX233-NAND/m-p/394103#M57623</guid>
      <dc:creator>federicodevitii</dc:creator>
      <dc:date>2015-10-13T19:24:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX233 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-NAND/m-p/394104#M57624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Federico&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one needs to add entries as shows attached file, so linux could recognize NAND.&lt;/P&gt;&lt;P&gt;Then mfg tools firmware should be rebuilt. For baremetal test one can reuse i.MX28 OBDS&lt;/P&gt;&lt;P&gt;GpmiNandReadId()&amp;nbsp; stmp_nand.c:&lt;/P&gt;&lt;P&gt;Lab and Test Software (1)&lt;/P&gt;&lt;P&gt;On-Board Diagnostic Suit for the i.MX28 (REV 1)&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX28 Evaluation Kit|Freescale&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 01:49:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX233-NAND/m-p/394104#M57624</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-10-14T01:49:19Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX233 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-NAND/m-p/394105#M57625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;i followed the istruction of User Guide for i.MX28 On-Board Diagnostics Suite (OBDS) for build a mx28-obds.sb file and flashed it on sd, but when boot a message appear on console &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Undefined Instruction&lt;/P&gt;&lt;P&gt;r14_un&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i tried to usb boot using sb_loader with the same results&lt;/P&gt;&lt;P&gt;after this i edited the build_mx28.sh script to chagne the elftosb option from "-f mx28" to "-f mx23" but at the end of building an error message say:&lt;/P&gt;&lt;P&gt;error: line 20: HAB features not supported with the selected family&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 19:09:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX233-NAND/m-p/394105#M57625</guid>
      <dc:creator>federicodevitii</dc:creator>
      <dc:date>2015-10-14T19:09:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX233 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-NAND/m-p/394106#M57626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Federico&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can run it with jtag&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Oct 2015 02:32:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX233-NAND/m-p/394106#M57626</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-10-15T02:32:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX233 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-NAND/m-p/394107#M57627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;loading other sb file (u-boot, linux kernel etc...) built for imx23 there is no problem with SD or USB. The problem is when i try to start MX28 OBDS on MX23 platform, because i think there is some instruction, like the HAB one, not supported from imx23&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Federico&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Oct 2015 07:41:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX233-NAND/m-p/394107#M57627</guid>
      <dc:creator>federicodevitii</dc:creator>
      <dc:date>2015-10-15T07:41:44Z</dc:date>
    </item>
  </channel>
</rss>