<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: pmic powerup problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/pmic-powerup-problem/m-p/393605#M57529</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;ok i will change to F0 part than i will come back to you and i went throgh AN4717 before design its fine&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Jul 2015 08:59:19 GMT</pubDate>
    <dc:creator>saida</dc:creator>
    <dc:date>2015-07-10T08:59:19Z</dc:date>
    <item>
      <title>pmic powerup problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pmic-powerup-problem/m-p/393601#M57525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi i.mx6 community&lt;/P&gt;&lt;P&gt;in my custom made board based on i.mx6 the pmic is not startsup&lt;/P&gt;&lt;P&gt;i am using pmic MMF0100NP device and when&amp;nbsp; power is given switch3 voltage 1.5v is coming remaining or not but standby signal is high&lt;/P&gt;&lt;P&gt;to make it low i shorted to ground through a jumper even voltages are not coming what could be the problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please can any one help me in this regsrd&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks and regards&lt;/P&gt;&lt;P&gt;saida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 12:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pmic-powerup-problem/m-p/393601#M57525</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2015-07-08T12:18:34Z</dc:date>
    </item>
    <item>
      <title>Re: pmic powerup problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pmic-powerup-problem/m-p/393602#M57526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;are you talking about 1V5 for DDR in pin 38?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reasons for that PS to miss are many:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- compare carefully the schematic with a similar board, as sabreauto maybe, well-known to work &lt;/P&gt;&lt;P&gt;- something wrong in the connected DDR, so once disconnected from the PMIC you should se the correct 1.5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also, never short pins directly to GND or VCC, always use a resistor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 13:46:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pmic-powerup-problem/m-p/393602#M57526</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2015-07-08T13:46:27Z</dc:date>
    </item>
    <item>
      <title>Re: pmic powerup problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pmic-powerup-problem/m-p/393603#M57527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;no i am getting DDR voltage from PMIC switch3 but problem is that reaminig i am not getting&lt;/P&gt;&lt;P&gt;one more thing is PMIC is getting hot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks and regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;saida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 17:25:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pmic-powerup-problem/m-p/393603#M57527</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2015-07-08T17:25:37Z</dc:date>
    </item>
    <item>
      <title>Re: pmic powerup problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pmic-powerup-problem/m-p/393604#M57528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI saida&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if chip is overheating it may turn off its supplies, recommended to&lt;/P&gt;&lt;P&gt;check connections using &lt;A href="http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf?fasp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;AN4717&lt;/A&gt; AN4717, Schematic Guidelines for the MMPF0100&lt;/P&gt;&lt;P&gt;Also MMF0100NP (not programmed) should not be used with i.MX6,&lt;/P&gt;&lt;P&gt;please use programmed parts, given in Table 1. Orderable Part Variations &lt;A href="http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;MMPF0100&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2015 01:06:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pmic-powerup-problem/m-p/393604#M57528</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-09T01:06:22Z</dc:date>
    </item>
    <item>
      <title>Re: pmic powerup problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pmic-powerup-problem/m-p/393605#M57529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;ok i will change to F0 part than i will come back to you and i went throgh AN4717 before design its fine&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jul 2015 08:59:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pmic-powerup-problem/m-p/393605#M57529</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2015-07-10T08:59:19Z</dc:date>
    </item>
  </channel>
</rss>