<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: iMX6 trace clock</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-trace-clock/m-p/393236#M57417</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"The Trace clocks are derived directly from the AHB clock. There is no ability &lt;/P&gt;&lt;P&gt;to change the trace clock frequencies other than changing the AHB clock &lt;/P&gt;&lt;P&gt;frequency, which will have multiple side effects in the system. So essentially, &lt;/P&gt;&lt;P&gt;no you cannot change the Trace clock frequency."&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 May 2015 03:09:30 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-05-26T03:09:30Z</dc:date>
    <item>
      <title>iMX6 trace clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-trace-clock/m-p/393235#M57416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using a Lauterbach debugger/trace on a iMX6 platform.&lt;/P&gt;&lt;P&gt;For an efficient tracing I would like to increase the trace clock, now it is set to 66 MHz. Optimum frequency would be something around 200 MHz..&lt;/P&gt;&lt;P&gt;Can someone kindly suggest me how to do that, the iMX6 Reference Manual doesn't help in this case.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2015 07:15:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-trace-clock/m-p/393235#M57416</guid>
      <dc:creator>lucaellero</dc:creator>
      <dc:date>2015-05-25T07:15:16Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 trace clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-trace-clock/m-p/393236#M57417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"The Trace clocks are derived directly from the AHB clock. There is no ability &lt;/P&gt;&lt;P&gt;to change the trace clock frequencies other than changing the AHB clock &lt;/P&gt;&lt;P&gt;frequency, which will have multiple side effects in the system. So essentially, &lt;/P&gt;&lt;P&gt;no you cannot change the Trace clock frequency."&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2015 03:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-trace-clock/m-p/393236#M57417</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-05-26T03:09:30Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 trace clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-trace-clock/m-p/393237#M57418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;thank you for your kind reply.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2015 14:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-trace-clock/m-p/393237#M57418</guid>
      <dc:creator>lucaellero</dc:creator>
      <dc:date>2015-05-27T14:28:42Z</dc:date>
    </item>
  </channel>
</rss>