<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCIMX6SLEVK Camera Interface in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX6SLEVK-Camera-Interface/m-p/393176#M57390</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. this depends on pad (which is used for such purpose), if it has LVE setting,&lt;/P&gt;&lt;P&gt;then it is possible&lt;/P&gt;&lt;P&gt;2. yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Apr 2015 09:41:28 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-04-10T09:41:28Z</dc:date>
    <item>
      <title>MCIMX6SLEVK Camera Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX6SLEVK-Camera-Interface/m-p/393173#M57387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently working with SoloLite EVK, I have few doubts on using the camera interface. The camera DOVDD is 1.8V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All the signals coming to the "Camera Expansion Connector - J24" are EPDC signals, so if not using EPD, can we enable the LVE field (1.8V mode) for the camera related signals, including the EPDC_GDRL (CSI_MCLK)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or do we need to provide 3.15V to 1.8V level translators in an add-on board ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Pankaj Rana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Apr 2015 13:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX6SLEVK-Camera-Interface/m-p/393173#M57387</guid>
      <dc:creator>pankajrana</dc:creator>
      <dc:date>2015-04-09T13:02:10Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX6SLEVK Camera Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX6SLEVK-Camera-Interface/m-p/393174#M57388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pankaj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think both solutions are possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2015 01:09:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX6SLEVK-Camera-Interface/m-p/393174#M57388</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-10T01:09:59Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX6SLEVK Camera Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX6SLEVK-Camera-Interface/m-p/393175#M57389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/igorpadykov"&gt;igorpadykov&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="CSI_MCLK.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49131i19D710EC5DE67AD9/image-size/large?v=v2&amp;amp;px=999" role="button" title="CSI_MCLK.jpg" alt="CSI_MCLK.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Since MCLK is provided by the CCM module directly, is it still possible to it in LVE mode ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. If it is possible to use configure LVE feature for Camera signals then we can directly wire up the Camera lines. Please confirm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pankaj Rana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2015 05:17:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX6SLEVK-Camera-Interface/m-p/393175#M57389</guid>
      <dc:creator>pankajrana</dc:creator>
      <dc:date>2015-04-10T05:17:21Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX6SLEVK Camera Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX6SLEVK-Camera-Interface/m-p/393176#M57390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. this depends on pad (which is used for such purpose), if it has LVE setting,&lt;/P&gt;&lt;P&gt;then it is possible&lt;/P&gt;&lt;P&gt;2. yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2015 09:41:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX6SLEVK-Camera-Interface/m-p/393176#M57390</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-10T09:41:28Z</dc:date>
    </item>
  </channel>
</rss>