<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Advanced controls of CSI camera in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Advanced-controls-of-CSI-camera/m-p/392856#M57350</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jerome,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you need to patch the capture.c to support them.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Jul 2015 14:44:28 GMT</pubDate>
    <dc:creator>SergioSolis</dc:creator>
    <dc:date>2015-07-09T14:44:28Z</dc:date>
    <item>
      <title>Advanced controls of CSI camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Advanced-controls-of-CSI-camera/m-p/392855#M57349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I add support for OV7742 (plugged on CSI port) on kernel 3.10.17. This camera is able to support banding filter and a few other useful features. These features are correctly supported by V4L API (see V4L2_CID_POWER_LINE_FREQUENCY, V4L2_CID_BAND_STOP_FILTER, ... ). However, mxc_v4l2_capture only forward a few subset of V4L controls to camera driver (see mxc_v4l2_s_ctrl() in mxc_v4l2_capture.c). Should I patch mxc_v4l2_capture.c in order to support them, or I have missed something?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Apr 2015 13:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Advanced-controls-of-CSI-camera/m-p/392855#M57349</guid>
      <dc:creator>jérômepouiller</dc:creator>
      <dc:date>2015-04-30T13:36:07Z</dc:date>
    </item>
    <item>
      <title>Re: Advanced controls of CSI camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Advanced-controls-of-CSI-camera/m-p/392856#M57350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jerome,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you need to patch the capture.c to support them.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2015 14:44:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Advanced-controls-of-CSI-camera/m-p/392856#M57350</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2015-07-09T14:44:28Z</dc:date>
    </item>
  </channel>
</rss>